Hi,
I’m playing around with Qspice (build dec 30,2024) and I am wondering why the FFT does not show the DC component of the signal
When I do not klick on “Keep DC component” the diagram looks like this:
and when I activate “keep DC component” the diagram looks like this:
In LTSpice, the FFT looks like this:
The DC component is visible and its value is 0db Volts, as expected.
What can I do to see the DC component in QSpice, too?
(In all cases I wanted to plot between 0Hz and 1kHz)