Hello,
Is it possible to provide an external reference clock to the DW3110 IC?
I’m planning to use the DW3110 for wireless hardware clock synchronization between ADCs. However, I’m having some difficulty providing a stable clock source that meets the DW3110’s requirements.
Ideally, I would like to use an external clock source so that the UWB IC and the ADCs can share or be referenced to the same clock. I’m planning to synthesise UWB and ADC clocks using the same PLL of Si5351 IC so both synthesized clocks are related.
Is this supported by the DW3110? If so, are there any specific requirements or recommended configurations for using an external clock?
Thanks!