Hi ,
I am using the EVKIT and i would like to connect a Raspberry Pi directly to the SPI of the DW1000.
i connected the straight forward SPI signals to the Raspberry pi (SDI, SDO, CSn & SCLK) , what should i do with the IRQn & WAKEUP signals ? ( they are disconnected from J6 …R41, R43)
- Do I need to connect the IRQ & WAKEUP to the Raspberry ?
- Is there any refernce code for this type of connection ?
Best regards
Dotan