Hi,
As per ETSI standard, the low duty cycle requirement states that the Sum transmitter ON time should be less than 18 s per hour. Whether this can be achieved in DW1000 projects. For achieving this the transmitter can be turned on only for maximum 5ms in a second. If we stick to this requirement, what will be the maximum refresh rate that we can achieve in TREK demo project?
Regards,
Shijo Thomas