Hi guys!
I need your help to check my code below. I have done several codes (1 tag and 3 anchors programs) using DW3000 Library from Makerfabs but it is not working properly. Why does it occur? And how to solve the incorrect distance value.
Here is the tag code:
#include “dw3000.h”
#define APP_NAME “DS TWR INIT v1.0”const uint8_t PIN_RST = 27;
const uint8_t PIN_IRQ = 34;
const uint8_t PIN_SS = 4;static dwt_config_t config = {
5,
DWT_PLEN_128,
DWT_PAC8,
9,
9,
1,
DWT_BR_6M8,
DWT_PHRMODE_STD,
DWT_PHRRATE_STD,
(128 + 1 + 8 - 8),
DWT_STS_MODE_OFF,
DWT_STS_LEN_64,
DWT_PDOA_M0
};#define RNG_DELAY_MS 100
#define TX_ANT_DLY 16387
#define RX_ANT_DLY 16387/For 1st Anchor/
static uint8_t tx_poll_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0x21};
static uint8_t rx_resp_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘V’, ‘E’, ‘W’, ‘A’, 0x10, 0x02, 0, 0};
static uint8_t tx_final_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};/For 2nd Anchor/
static uint8_t tx_poll_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘A’, ‘C’, ‘R’, ‘2’, 0x21, 0, 0};
static uint8_t rx_resp_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘R’, ‘2’, ‘A’, ‘C’, 0x10, 0x02, 0, 0, 0, 0};
static uint8_t tx_final_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘A’, ‘C’, ‘R’, ‘2’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};/For 3rd Anchor/
static uint8_t tx_poll_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘S’, ‘N’, ‘Y’, ‘L’, 0x21, 0, 0};
static uint8_t rx_resp_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘Y’, ‘L’, ‘S’, ‘N’, 0x10, 0x02, 0, 0, 0, 0};
static uint8_t tx_final_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘S’, ‘N’, ‘Y’, ‘L’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};#define ALL_MSG_COMMON_LEN_1 10
#define ALL_MSG_COMMON_LEN_2 10
#define ALL_MSG_COMMON_LEN_3 10#define ALL_MSG_SN_IDX_1 2
#define ALL_MSG_SN_IDX_2 2
#define ALL_MSG_SN_IDX_3 2#define FINAL_MSG_POLL_TX_TS_IDX_1 10
#define FINAL_MSG_POLL_TX_TS_IDX_2 10
#define FINAL_MSG_POLL_TX_TS_IDX_3 10#define FINAL_MSG_RESP_RX_TS_IDX_1 14
#define FINAL_MSG_RESP_RX_TS_IDX_2 14
#define FINAL_MSG_RESP_RX_TS_IDX_3 14#define FINAL_MSG_FINAL_TX_TS_IDX_1 18
#define FINAL_MSG_FINAL_TX_TS_IDX_2 18
#define FINAL_MSG_FINAL_TX_TS_IDX_3 18static uint8_t frame_seq_nb_1 = 0;
static uint8_t frame_seq_nb_2 = 0;
static uint8_t frame_seq_nb_3 = 0;#define RX_BUF_LEN_1 20
static uint8_t rx_buffer_1[RX_BUF_LEN_1];#define RX_BUF_LEN_2 20
static uint8_t rx_buffer_2[RX_BUF_LEN_2];#define RX_BUF_LEN_3 20
static uint8_t rx_buffer_3[RX_BUF_LEN_3];static uint32_t status_reg_1 = 0;
static uint32_t status_reg_2 = 0;
static uint32_t status_reg_3 = 0;#define POLL_TX_TO_RESP_RX_DLY_UUS 700
#define RESP_RX_TO_FINAL_TX_DLY_UUS 700
#define RESP_RX_TIMEOUT_UUS 300
#define PRE_TIMEOUT 5
static double tof_1;
static double distance_1;static double tof_2;
static double distance_2;static double tof_3;
static double distance_3;static uint64_t poll_tx_ts_1;
static uint64_t resp_rx_ts_1;
static uint64_t final_tx_ts_1;static uint64_t poll_tx_ts_2;
static uint64_t resp_rx_ts_2;
static uint64_t final_tx_ts_2;static uint64_t poll_tx_ts_3;
static uint64_t resp_rx_ts_3;
static uint64_t final_tx_ts_3;extern dwt_txconfig_t txconfig_options;
/*! ---------------------------------------------------------------------------
- @fn ds_twr_initiator()
- @brief Application entry point.
- @param none
- @return none
*/void setup()
{
UART_init();
test_run_info((unsigned char *)APP_NAME);
spiBegin(PIN_IRQ, PIN_RST);
spiSelect(PIN_SS);Sleep(2); while (!dwt_checkidlerc()) { UART_puts("IDLE FAILED\r\n"); while (1); } if (dwt_initialise(DWT_DW_INIT) == DWT_ERROR) { UART_puts("INIT FAILED\r\n"); //LOG_INF("INIT FAILED"); while (1) { /* spin */ }; } if (dwt_configure(&config)) { UART_puts("CONFIG FAILED\r\n"); //LOG_INF("CONFIG FAILED"); while (1) { /* spin */ }; } dwt_configuretxrf(&txconfig_options); dwt_setrxantennadelay(RX_ANT_DLY); dwt_settxantennadelay(TX_ANT_DLY); dwt_setrxaftertxdelay(POLL_TX_TO_RESP_RX_DLY_UUS); dwt_setrxtimeout(RESP_RX_TIMEOUT_UUS); dwt_setpreambledetecttimeout(PRE_TIMEOUT); dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE); dwt_setleds(DWT_LEDS_ENABLE | DWT_LEDS_INIT_BLINK);}
void loop(){
/1st Anchor Program/
while(1){
tx_poll_msg_1[ALL_MSG_SN_IDX_1] = frame_seq_nb_1;
dwt_writetxdata(sizeof(tx_poll_msg_1), tx_poll_msg_1, 0);
dwt_writetxfctrl(sizeof(tx_poll_msg_1)+FCS_LEN, 0, 1);dwt_starttx(DWT_START_TX_IMMEDIATE | DWT_RESPONSE_EXPECTED); while (!((status_reg_1 = dwt_read32bitreg(SYS_STATUS_ID)) & (SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR))){ /* spin */ }; frame_seq_nb_1++; if (status_reg_1 & SYS_STATUS_RXFCG_BIT_MASK){ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_TXFRS_BIT_MASK); uint32_t frame_len_1 = dwt_read32bitreg(RX_FINFO_ID) & FRAME_LEN_MAX_EX; if (frame_len_1 <= RX_BUF_LEN_1){ dwt_readrxdata(rx_buffer_1, frame_len_1, 0); } rx_buffer_1[ALL_MSG_SN_IDX_1] = 0; if (memcmp(rx_buffer_1, rx_resp_msg_1, ALL_MSG_COMMON_LEN_1) == 0){ uint32_t final_tx_time_1; poll_tx_ts_1 = get_tx_timestamp_u64(); resp_rx_ts_1 = get_rx_timestamp_u64(); final_tx_time_1 = (resp_rx_ts_1 + (RESP_RX_TO_FINAL_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8; dwt_setdelayedtrxtime(final_tx_time_1); final_tx_ts_1 = (((uint64_t)(final_tx_time_1 & 0xFFFFFFFEUL)) << 8) + TX_ANT_DLY; final_msg_set_ts(&tx_final_msg_1[FINAL_MSG_POLL_TX_TS_IDX_1], poll_tx_ts_1); final_msg_set_ts(&tx_final_msg_1[FINAL_MSG_RESP_RX_TS_IDX_1], resp_rx_ts_1); final_msg_set_ts(&tx_final_msg_1[FINAL_MSG_FINAL_TX_TS_IDX_1], final_tx_ts_1); tx_final_msg_1[ALL_MSG_SN_IDX_1] = frame_seq_nb_1; dwt_writetxdata(sizeof(tx_final_msg_1), tx_final_msg_1, 0); /* Zero offset in TX buffer. */ dwt_writetxfctrl(sizeof(tx_final_msg_1)+FCS_LEN, 0, 1); /* Zero offset in TX buffer, ranging bit set. */ int ret_1 = dwt_starttx(DWT_START_TX_DELAYED); if (ret_1 == DWT_SUCCESS) { while (!(dwt_read32bitreg(SYS_STATUS_ID) & SYS_STATUS_TXFRS_BIT_MASK)){ /* spin */ }; dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_TXFRS_BIT_MASK); frame_seq_nb_1++; } } } else{ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR | SYS_STATUS_TXFRS_BIT_MASK); }}
/Achors 2 Program/
while(1){
tx_poll_msg_2[ALL_MSG_SN_IDX_2] = frame_seq_nb_2;
dwt_writetxdata(sizeof(tx_poll_msg_2), tx_poll_msg_2, 0);
dwt_writetxfctrl(sizeof(tx_poll_msg_2)+FCS_LEN, 0, 1);dwt_starttx(DWT_START_TX_IMMEDIATE | DWT_RESPONSE_EXPECTED); while (!((status_reg_2 = dwt_read32bitreg(SYS_STATUS_ID)) & (SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR))){ /* spin */ }; frame_seq_nb_2++; if (status_reg_2 & SYS_STATUS_RXFCG_BIT_MASK){ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_TXFRS_BIT_MASK); uint32_t frame_len_2 = dwt_read32bitreg(RX_FINFO_ID) & FRAME_LEN_MAX_EX; if (frame_len_2 <= RX_BUF_LEN_2){ dwt_readrxdata(rx_buffer_2, frame_len_2, 0); } rx_buffer_2[ALL_MSG_SN_IDX_2] = 0; if (memcmp(rx_buffer_2, rx_resp_msg_2, ALL_MSG_COMMON_LEN_2) == 0){ uint32_t final_tx_time_2; poll_tx_ts_2 = get_tx_timestamp_u64(); resp_rx_ts_2 = get_rx_timestamp_u64(); final_tx_time_2 = (resp_rx_ts_2 + (RESP_RX_TO_FINAL_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8; dwt_setdelayedtrxtime(final_tx_time_2); final_tx_ts_2 = (((uint64_t)(final_tx_time_2 & 0xFFFFFFFEUL)) << 8) + TX_ANT_DLY; final_msg_set_ts(&tx_final_msg_2[FINAL_MSG_POLL_TX_TS_IDX_2], poll_tx_ts_2); final_msg_set_ts(&tx_final_msg_2[FINAL_MSG_RESP_RX_TS_IDX_2], resp_rx_ts_2); final_msg_set_ts(&tx_final_msg_2[FINAL_MSG_FINAL_TX_TS_IDX_2], final_tx_ts_2); tx_final_msg_2[ALL_MSG_SN_IDX_2] = frame_seq_nb_2; dwt_writetxdata(sizeof(tx_final_msg_2), tx_final_msg_2, 0); dwt_writetxfctrl(sizeof(tx_final_msg_2)+FCS_LEN, 0, 1); int ret_2 = dwt_starttx(DWT_START_TX_DELAYED); if (ret_2 == DWT_SUCCESS) { while (!(dwt_read32bitreg(SYS_STATUS_ID) & SYS_STATUS_TXFRS_BIT_MASK)){ /* spin */ }; dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_TXFRS_BIT_MASK); frame_seq_nb_2++; } } } else{ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR | SYS_STATUS_TXFRS_BIT_MASK); }}
/3rd Anchor Program/
while(1){
tx_poll_msg_1[ALL_MSG_SN_IDX_3] = frame_seq_nb_3;
dwt_writetxdata(sizeof(tx_poll_msg_3), tx_poll_msg_3, 0);
dwt_writetxfctrl(sizeof(tx_poll_msg_3)+FCS_LEN, 0, 1);
dwt_starttx(DWT_START_TX_IMMEDIATE | DWT_RESPONSE_EXPECTED);
while (!((status_reg_3 = dwt_read32bitreg(SYS_STATUS_ID)) &
(SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO |
SYS_STATUS_ALL_RX_ERR))){ /* spin */ };frame_seq_nb_3++; if (status_reg_3 & SYS_STATUS_RXFCG_BIT_MASK){ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_TXFRS_BIT_MASK); uint32_t frame_len_3 = dwt_read32bitreg(RX_FINFO_ID) & FRAME_LEN_MAX_EX; if (frame_len_3 <= RX_BUF_LEN_3){ dwt_readrxdata(rx_buffer_3, frame_len_3, 0); } rx_buffer_3[ALL_MSG_SN_IDX_3] = 0; if (memcmp(rx_buffer_3, rx_resp_msg_3, ALL_MSG_COMMON_LEN_3) == 0){ uint32_t final_tx_time_3; poll_tx_ts_3 = get_tx_timestamp_u64(); resp_rx_ts_3 = get_rx_timestamp_u64(); final_tx_time_3 = (resp_rx_ts_3 + (RESP_RX_TO_FINAL_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8; dwt_setdelayedtrxtime(final_tx_time_3); final_tx_ts_3 = (((uint64_t)(final_tx_time_3 & 0xFFFFFFFEUL)) << 8) + TX_ANT_DLY; final_msg_set_ts(&tx_final_msg_3[FINAL_MSG_POLL_TX_TS_IDX_3], poll_tx_ts_3); final_msg_set_ts(&tx_final_msg_3[FINAL_MSG_RESP_RX_TS_IDX_3], resp_rx_ts_3); final_msg_set_ts(&tx_final_msg_3[FINAL_MSG_FINAL_TX_TS_IDX_3], final_tx_ts_3); tx_final_msg_1[ALL_MSG_SN_IDX_3] = frame_seq_nb_3; dwt_writetxdata(sizeof(tx_final_msg_3), tx_final_msg_3, 0); dwt_writetxfctrl(sizeof(tx_final_msg_3)+FCS_LEN, 0, 1); int ret_3 = dwt_starttx(DWT_START_TX_DELAYED); if (ret_3 == DWT_SUCCESS) { while (!(dwt_read32bitreg(SYS_STATUS_ID) & SYS_STATUS_TXFRS_BIT_MASK)){ /* spin */ }; dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_TXFRS_BIT_MASK); frame_seq_nb_3++; } } } else{ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR | SYS_STATUS_TXFRS_BIT_MASK); }}
Sleep(RNG_DELAY_MS);
}
Here is the 1st anchor program:
#include “dw3000.h”
#define APP_NAME “DS TWR RESP_1 v1.0”const uint8_t PIN_RST = 27;
const uint8_t PIN_IRQ = 34;
const uint8_t PIN_SS = 4;static dwt_config_t config = {
5,
DWT_PLEN_128,
DWT_PAC8,
9,
9,
1,
DWT_BR_6M8,
DWT_PHRMODE_STD,
DWT_PHRRATE_STD,
(128 + 1 + 8 - 8),
DWT_STS_MODE_OFF,
DWT_STS_LEN_64,
DWT_PDOA_M0
};#define RNG_DELAY_MS 100
#define TX_ANT_DLY 0
#define RX_ANT_DLY 0 //16385/For 1st Anchor/
static uint8_t rx_poll_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0x21, 0, 0};
static uint8_t tx_resp_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘V’, ‘E’, ‘W’, ‘A’, 0x10, 0x02, 0, 0, 0, 0};
static uint8_t rx_final_msg_1 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};#define ALL_MSG_COMMON_LEN_1 10
#define ALL_MSG_SN_IDX_1 2
#define FINAL_MSG_POLL_TX_TS_IDX_1 10
#define FINAL_MSG_RESP_RX_TS_IDX_1 14
#define FINAL_MSG_FINAL_TX_TS_IDX_1 18static uint8_t frame_seq_nb_1 = 0;
#define RX_BUF_LEN_1 24
static uint8_t rx_buffer_1[RX_BUF_LEN_1];
static uint32_t status_reg_1 = 0;
#define POLL_RX_TO_RESP_TX_DLY_UUS 900
#define RESP_TX_TO_FINAL_RX_DLY_UUS 500
#define FINAL_RX_TIMEOUT_UUS 220
#define PRE_TIMEOUT 5static uint64_t poll_rx_ts_1;
static uint64_t resp_tx_ts_1;
static uint64_t final_rx_ts_1;static double tof_1;
static double distance_1;extern dwt_txconfig_t txconfig_options;
/*! ---------------------------------------------------------------------------
- @fn ds_twr_responder()
- @brief Application entry point.
- @param none
- @return none
*/void setup()
{
UART_init();
test_run_info((unsigned char *)APP_NAME);
spiBegin(PIN_IRQ, PIN_RST);
spiSelect(PIN_SS);Sleep(2);
while (!dwt_checkidlerc()) {
UART_puts(“IDLE FAILED\r\n”);
while (1) ;
};if (dwt_initialise(DWT_DW_INIT) == DWT_ERROR) { while (1) { /* spin */ }; } if (dwt_configure(&config)) { // LOG_ERR("CONFIG FAILED"); while (1) { /* spin */ }; } dwt_configuretxrf(&txconfig_options); dwt_setrxantennadelay(RX_ANT_DLY); dwt_settxantennadelay(TX_ANT_DLY); dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE); dwt_setleds(DWT_LEDS_ENABLE | DWT_LEDS_INIT_BLINK);}
/* Loop forever responding to ranging requests. */
void loop (){
while (1){
dwt_setpreambledetecttimeout(0);
dwt_setrxtimeout(0);
dwt_rxenable(DWT_START_RX_IMMEDIATE);while (!((status_reg_1 = dwt_read32bitreg(SYS_STATUS_ID)) & (SYS_STATUS_RXFCG_BIT_MASK |SYS_STATUS_ALL_RX_TO |SYS_STATUS_ALL_RX_ERR))){ /* spin */ }; if (status_reg_1 & SYS_STATUS_RXFCG_BIT_MASK){ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK); uint32_t frame_len_1 = dwt_read32bitreg(RX_FINFO_ID) & FRAME_LEN_MAX_EX; if (frame_len_1 <= RX_BUF_LEN_1){ dwt_readrxdata(rx_buffer_1, frame_len_1, 0); } rx_buffer_1[ALL_MSG_SN_IDX_1] = 0; if (memcmp(rx_buffer_1, rx_poll_msg_1, ALL_MSG_COMMON_LEN_1) == 0){ uint32_t resp_tx_time_1; poll_rx_ts_1 = get_rx_timestamp_u64(); resp_tx_time_1 = (poll_rx_ts_1 + (POLL_RX_TO_RESP_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8; dwt_setdelayedtrxtime(resp_tx_time_1); dwt_setrxaftertxdelay(RESP_TX_TO_FINAL_RX_DLY_UUS); dwt_setrxtimeout(FINAL_RX_TIMEOUT_UUS); dwt_setpreambledetecttimeout(PRE_TIMEOUT); tx_resp_msg_1[ALL_MSG_SN_IDX_1] = frame_seq_nb_1; dwt_writetxdata(sizeof(tx_resp_msg_1), tx_resp_msg_1, 0); /* Zero offset in TX buffer. */ dwt_writetxfctrl(sizeof(tx_resp_msg_1), 0, 1); /* Zero offset in TX buffer, ranging. */ int ret = dwt_starttx(DWT_START_TX_DELAYED | DWT_RESPONSE_EXPECTED); if (ret == DWT_ERROR){ continue; } while (!((status_reg_1 = dwt_read32bitreg(SYS_STATUS_ID)) & (SYS_STATUS_RXFCG_BIT_MASK |SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR))){ /* spin */ }; frame_seq_nb_1++; if (status_reg_1 & SYS_STATUS_RXFCG_BIT_MASK) { dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_TXFRS_BIT_MASK); frame_len_1 = dwt_read32bitreg(RX_FINFO_ID) & FRAME_LEN_MAX_EX; if (frame_len_1 <= RX_BUF_LEN_1){ dwt_readrxdata(rx_buffer_1, frame_len_1, 0); } rx_buffer_1[ALL_MSG_SN_IDX_1] = 0; if (memcmp(rx_buffer_1, rx_final_msg_1, ALL_MSG_COMMON_LEN_1) == 0){ uint32_t poll_tx_ts_1, resp_rx_ts_1, final_tx_ts_1; uint32_t poll_rx_ts_1, resp_tx_ts_1, final_rx_ts_1; double Ra_1, Rb_1, Da_1, Db_1; int64_t tof_dtu_1; resp_tx_ts_1 = get_tx_timestamp_u64(); final_rx_ts_1 = get_rx_timestamp_u64(); final_msg_get_ts(&rx_buffer_1[FINAL_MSG_POLL_TX_TS_IDX_1], &poll_tx_ts_1); final_msg_get_ts(&rx_buffer_1[FINAL_MSG_RESP_RX_TS_IDX_1], &resp_rx_ts_1); final_msg_get_ts(&rx_buffer_1[FINAL_MSG_FINAL_TX_TS_IDX_1], &final_tx_ts_1); poll_rx_ts_1 = (uint32_t)poll_rx_ts_1; resp_tx_ts_1 = (uint32_t)resp_tx_ts_1; final_rx_ts_1= (uint32_t)final_rx_ts_1; Ra_1 = (double)(resp_rx_ts_1 - poll_tx_ts_1); Rb_1 = (double)(final_rx_ts_1 - resp_tx_ts_1); Da_1 = (double)(final_tx_ts_1 - resp_rx_ts_1); Db_1 = (double)(resp_tx_ts_1 - poll_rx_ts_1); tof_dtu_1 = (int64_t)((Ra_1 * Rb_1 - Da_1 * Db_1) / (Ra_1 + Rb_1 + Da_1 + Db_1)); tof_1 = tof_dtu_1 * DWT_TIME_UNITS; distance_1 = tof_1 * SPEED_OF_LIGHT; char dist[20] = {0}; snprintf(dist_str, sizeof(dist_str), "distance 1: %3.2f m ", distance_1); test_run_info((unsigned char *)dist_str); Serial.println("0 "+String(distance_1)); Sleep(RNG_DELAY_MS - 10); // start couple of ms earlier } } else { dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR); } } } else{ dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR); }}
}
Here is the 2nd anchor program:
the same code as 1st anchor code, but the difference in this part of the code:
/For 2nd Anchor/
static uint8_t rx_poll_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘A’, ‘C’, ‘R’, ‘2’, 0x21, 0, 0};
static uint8_t tx_resp_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘R’, ‘2’, ‘A’, ‘C’, 0x10, 0x02, 0, 0, 0, 0};
static uint8_t rx_final_msg_2 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘A’, ‘C’, ‘R’, ‘2’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};
Here is the 3rd anchor program:
the same code as 1st anchor code, but the difference in this part of the code:
/For 3rd Anchor/
static uint8_t rx_poll_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘S’, ‘N’, ‘Y’, ‘L’, 0x21, 0, 0};
static uint8_t tx_resp_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘Y’, ‘L’, ‘S’, ‘N’, 0x10, 0x02, 0, 0, 0, 0};
static uint8_t rx_final_msg_3 = {0x41, 0x88, 0, 0xCA, 0xDE, ‘S’, ‘N’, ‘Y’, ‘L’, 0x23, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};