Good morning everyone,
Quick introduction and background - I primarily work in SQL databases and dabble in C# so embedded systems is completely outside my forte; however, I’m intrigued to learn how to setup an UWB transceiver as I have been developing a digital twin software for a couple of years as a hobby and I want to do near-real time tracking within it. I’m heavily leveraging AI to speed up my workflow trying to get up to speed on the DWM3001CDK. I purchased two of them roughly a month ago. In that time I’ve successfully gotten the RTT, Shell, LEDs, and Accelerometer functioning. For one brief moment I actually succeeded in getting a Device ID read off my DW3000 before it went into sleep mode I think because my CoPilot chat history tells me I did but I must’ve missed it when fumbling through all the code tweaks. That was two weeks ago and I’ve been getting nothing but 0x0000000 since then. For all the great speed enhancements AI has given me, one catch is that once it exhausts everything it knows it starts to get into rabbit holes. It was convinced my pin mapping was incorrect. I’ll share below what I have as I’m pretty sure I’m reading the schematic properly. I’ve been following the SDK guide and having the AI tools help me develop API calls to the DW3000 to initialize, etc.
If anyone has successfully gotten their Device ID read on DWM3001CDK_C2 using Zephyr + SDK Drivers I’d appreciate any advice or assistance. Let me know if you need to see my repo or any specific part of my project.
Slowly making more progress after another two days reading through docs and driver pointers. My Temperature check was failing and getting stuck in an infinite loop so had to disable it in both initialise and configure API calls. Appears my configure failed and CoPilot is questioning my pins or the logic I’m using for wake up.
/* --------------------------------------------------------------------------
* Wakeup callback (driver will call this during dwt_initialise)
* -------------------------------------------------------------------------- */
static void dw3000_wakeup_ic_zephyr(void)
{
gpio_pin_configure_dt(&cs_gpio, GPIO_OUTPUT);
gpio_pin_set_dt(&cs_gpio, 0);
k_sleep(K_USEC(700));
gpio_pin_set_dt(&cs_gpio, 1);
k_sleep(K_MSEC(2));
gpio_pin_configure_dt(&cs_gpio, GPIO_INPUT);
}
@Wassim_Qorvo,
I saw a comment from you on this post (Getting started with DWM3001CDKE - #8 by Wassim_Qorvo) stating that GPIO 1, 19 is the wakeup pin for DW3000. Does DWM3001CDK_C2 actually have an accessible wakeup pin? When I try to access 1, 19 I get the following on RTT.
The CS assert when I try to force the pins and read back their values appears to not show pin movement so it’s almost like my DW3000 won’t allow me to drive GPIO to wake it.
I downloaded the SDK (DW3_QM33_SDK_1.1.1) and the Release_Notes.pdf contains (DW3110) in the supported chip list. I don’t find this chip in the deca_device_api.h. My device ID read is coming back as 0xBC950704 which I’m finding documented nowhere currently. It seems I cannot get TX working properly. RX works somehow using the DW3000 driver because I can “listen” and decode plenty of things in the local area but I’m not “hearing” my TX board speak to my RX board. Does anyone have advice on next steps?
I pitted CoPilot against Gemini to help diagnose the issue. Turns out Gemini is really intelligent regarding leading edge clock and bit shifting errors. I showed CoPilot what I got and it swore I had an undocumented Qorvo chip. Gemini corrected that assumption and proved I had a timing issue. Apparently I shouldn’t have been calling CPHA because by calling it in config it sets to 1 and changing my SPI mode. Once I removed that I got a clean read output on RTT.
Good evening everyone.
I have not made much progress since my last post. 9 Days and still trying to get legit UWB RX working. I either see a sea of “A” or a sea of “0”. I think I’m reading a loop of the same data so will continue troubleshooting. Would love advice if anyone has their DWM3001CDK_C2 running in Zephyr using the SDK. My current goal is to get TWR up and running between my two boards. If someone’s got a working trimmed down example or wants to take my current project to help me figure out what I need to fix, I’ll gladly pay for your time.
I saw your tutorials—excellent work and very helpful for the community.
The examples in your tutorial from the SDK primarily use the dw_ API for low-level transceiver control. Have you ever had success in linking the supplied FiRa-compliant libraries, the QAIN (Qorvo Architecture Integration Layer) library, and successfully calling the QSOL (Qorvo Stack Orchestration Layer)?
I’m looking to move beyond the basic 802.15.4z pulses and leverage the full secure ranging stack, but the integration between the pre-compiled Qorvo blobs and the Zephyr environment can be quite a hurdle.
@leapslabs Following up on @narfster’s question; using your QM33120WDK2 dev kit would be great, but if the higher-level FiRa/QAIN/QSOL stacks aren’t supported, that kind of defeats the purpose of using these high-end chips (that come with complete SDKs).
The UDK SDK does not support development of the FiRa compatible application.
But you can check the Qorvo Nearby Interaction SDK and possibly use that framework to develop FiRa compatible application for the Murata 2AB module, which is used on the QM33120WDK2 kit.