DWM3001CDK UCI Flash Bad

After two computers and various settings, I can’t get DWM3001CDK-UCI-FreeRTOS.hex to work at all. It works with CLI version, but the UCI seems to have issues. Can we get the source code and compile it ourselves?

Or a new hex file made?

Thanks!

Hi @zebra105s , which SDK are you using? What seems to be the issue? Is the flashing failing? Please share any screenshots to help us further debug.

DW3_QM33_SDK_1.1.1, fresh download today 9/16/2025.

The Erase and flash go fine. When you change over to the com port, it’s not responsive. I can erase and flash as CLI and it works, but I’m shooting for UCI!

DW3_QM33_SDK_1.1.1, fresh download today 9/16/2025.

The Erase and flash go fine. When you change over to the com port, it’s not responsive. I can erase and flash as CLI and it works, but I’m shooting for UCI!

@zebra105s , did you change the USB port on the DWM3001CDK after flashing? Please also share a screenshot of device manager with the USB cable plugged into the USB port closer to the antenna.