Hi,
I am planning to use the DWM3001CDK outdoors, installed inside a protective enclosure and exposed to direct sunlight.
I would like to better understand the thermal limitations of the complete DWM3001CDK, not only the DWM3001C module itself.
I found that the DWM3001C module has an operating temperature range of -40 °C to +85 °C, but I have a few questions regarding the complete development board and its installation inside an enclosure:
What is the recommended operating temperature range for the complete DWM3001CDK board, including all onboard components?
Does the DWM3001CDK generate any significant heat during continuous operation, especially when performing frequent UWB ranging and communication?
For outdoor use in direct sunlight, what internal enclosure temperature would be considered safe for long-term continuous operation?
What enclosure materials are recommended in order to minimize attenuation, reflection, or distortion of the UWB?
Before considering the thermal and enclosure aspects, please note that in the US, FCC rules do not generally permit UWB operation as fixed outdoor infrastructure. Fixed outdoor UWB installations require specific regulatory consideration, such as an FCC waiver. Handheld UWB devices may operate outdoors, but this does not extend to fixed outdoor infrastructure. Please refer to FCC 47 CFR §15.519.
Regarding the hardware, the DWM3001C module itself is specified for -40 °C to +85 °C operation. The DWM3001CDK, however, is an evaluation/development board and does not have a separately specified operating-temperature range for the complete board assembly.
For an outdoor enclosure, the main thermal concern would typically be solar loading rather than self-heating from the UWB circuitry. The actual internal temperature should be measured under the intended environmental and operating conditions, with sufficient margin maintained below the temperature limits of all components.
For the enclosure material, non-conductive RF-transparent plastics are generally preferred. Metal or conductive materials should be avoided near the UWB antenna. Enclosure material, thickness, and spacing from the antenna can affect antenna impedance and radiation pattern, so RF performance should be verified in the final enclosure.
For a production design, we recommend designing around the DWM3001C module rather than using the DWM3001CDK as the final hardware.