DWM3001CDK tag and anchor setup, tag stops sending values after about 5 minutes

Hello, first post on here, apologies if I miss any forum etiquette.

I’m trying to setup a UWB localisation system using the DWM3001CDK. I have four of the boards, each attached to a Raspberry Pi Zero 2 W, acting as the anchors, and one board acting as the tag. I am using this Git Repo GitHub - b4shful/uwb_app · GitHub to make the system. At the moment, the system runs completely fine for about 5 minutes, and then the tag suddenly stops communicating any data. Any idea why this would be happening?

Thank you in advance :slight_smile:

what firmware is loaded onto the CDK boards? (which SDK version?)

hello, apologies for the delay.

i think it’s DW3_QM33_SDK_1.1.1.