Dwm3001cdk sdk programming using flasher lite

I want to program the Dwm3001cdk module I tried to connect with j flash lite but in the log shows can’t connect to the device and it shows No probe via usb is connected and after that how to upload program for that can anyone explain please

Hi @jayakandan,

Please make sure you are connecting to the correct USB port for programming. It should be the one that is further away from the antenna. If it is still not working, please share a screenshot of Device Manager while you have the cable connected.

I solve this problem by downloading the lower version of the j flash lite i upload the firmware now i want to upload the code to detect from qorov app to see distansce and angle elevation

How are you looking to do the ranging? Are you looking to use the DWM3001CDK with an iPhone or 2 DWM3001CDKs connected to your computer?

yes i would like to do ranging from the iphone,you have any idea to do that,if its explain

For ranging to the iPhone, then you should use the Nearby Interaction example from the latest SDK. Then on the phone side you will see the angle and distance.

yeah i have done that,in nrf connect app it is showing as normal ble i want to program them as the ibeacon and the uwb want to show on qorov app an the without connect option can we see the distance from the iphone if it is nearby

is there any source code for the “DWM3001CDK-QANI-FreeRTOS.hex”,for this hex file and how to get the hex file,is there any way to do that

i want to integerate ibeacon as well the uwb can i do that,how can we do that both

The 3001cdk board is UWB only.
Two different firmware

Nearby, use with iPhone (QANI)
Fira, use usb connect to computer, run script on both sides

Example app for both

yes in the zip file at

Qorvo_Nearby_Interaction_3_2_1/Software/Accessory/Sources

unzip the zipfile there to get the source tree

 ls
QANI-All-FreeRTOS_QNI_3_0_0	QANI-All-FreeRTOS_QNI_3_0_0.zip