I am working with the DWM3001CDK module through serial port (command line interface firmware). The issue is that I get the distance values between the tag and the anchor but I only get that and the value of the Crystal frequency Offset (CFO_100ppm). All the other values are always equal to zero. Since the module loses measurement precision depending on the angle, I would need these other values in order to work around the precision problem. Can someone please help me solve this ?
It should be a mistake and copied from QM33120WDK1 Developer guide.
Using QM33120WDK1 (containing one Aoa and one non Aoa board), you should be able to get the angle
Thank you @wassim for the explanations. I took a look at the module and the antennas would have to face each other for the duration of the measurements. But by the use I want to make of it, I will have to be able to rotate with the tag and still have the good distance values. Can you recommend a module that can do the job?