Hi everyone,
I’m studying the performance of CIR by doing several experiments at different distances. I’ve only done LOS so far but I should also do NLOS. I need help estimating the delay. I show you in the figures below what I get for the CIR at 145 cm and 300 cm and in particular the highest peak that I think is related to packets/ signals received without reflection. What I suppose will happen when I do the same experiments at the same distances but in the NLOS case is that I will have the peaks moved. But what I would like to know is the delay that is observed. From here I should be able to calculate the reflections.
Can someone help me?
Thank You in advance.
kind Regards,
Antonello