I’m using the DWM3001CDK boards in a 1 (Tag–Initiator) : N (Anchor–Responder) setup. My goal is for the Tag board to measure distances to each Anchor and then send those distance values to a smartphone over BLE for trilateration.
I’m following this open‑source project and, for measurement convenience, plan to assign different device IDs to Tag and Anchor so I can build separate prebuilt binaries for each:
While 1:1 communication works perfectly, as soon as I switch to 1:2 the second board fails to complete its distance measurement. The logs show the RESP message is sent correctly, but on the INIT side I see:
[00:00:21.539,520] <inf> SIT_DISTANCE: Test: 03a000f7 & 00004000
[00:00:21.539,672] <wrn> SIT_DISTANCE: sit_checkReceivedMessage() no 'RX Frame Checksum Good'
[00:00:21.539,733] <wrn> SIT_DISTANCE: sit_checkReceivedMessage() reg1 = 0x03a000f7 ; reg2 = 0x038000f7 ; removed = 0x00200000
[00:00:21.539,825] <err> SIT_DISTANCE: sit_checkReceivedIdFinalMsg(1, header) fail
[00:00:21.539,855] <wrn> SIT_Module: Something is wrong
From inspecting the code, it seems the bitwise AND between the received status register and DWT_INT_RXFCG_BIT_MASK is never true:
waitForSysStatus(&l_status_reg, NULL,
(DWT_INT_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR), 0);
I don’t have much UWB experience, so I’m finding it hard to debug. Any hints or pointers would be greatly appreciated.
For reference, here are my build‑time settings (see lib/sit/sit.c in the repo):
#if defined(CONFIG_DEVICE_INITF)
device_settings.device_type = initiator;
device_settings.initiator = 1;
device_settings.responder = 101;
device_settings.devices = 2;
#elif defined(CONFIG_DEVICE_RESPF)
device_settings.device_type = responder;
device_settings.initiator = 0;
device_settings.responder = 0;
#else
LOG_ERR("Define DEVICE_INITF or DEVICE_RESPF");
#endif
device_settings.measurement_type = ss_twr;
device_settings.state = measurement;
device_settings.deviceID = CONFIG_DEVICE_ID;
device_type = device_settings.device_type;
Thank you in advance for any advice!