I have a dwm3000evb board with arduino headers, and an nRF52840-dk. I’ve downloaded the DWS3000 Software and API Guide and followed the README_nRF52840-DK.txt file exactly, including downloading the nRF SDK v16.0.0 and modifying the .emProject file. However, when I click “build and run”, the build fails and the following error message is output:
Building ‘dw3000_api’ from solution ‘dw3000_api’ in configuration ‘Debug
...
Compiling ‘SEGGER_RTT_Syscalls_SES.c’
__vfprintf.h: No such file or directory
...
Build failed
My understanding was that Segger Embedded Studio comes with the standard library. Is this somehow missing or was there a configuration step that I’m not familiar with here?
This is probably a really dumb mistake, but I’d appreciate any input or help.
Thanks!
I have the same error message with the same file with my Nordic SDK 17.0 project.
But only after updating from Segger Studio 5.70a to Segger Studio 6.20.
I think there are no public releases of Segger Studio between these two versions, so the new version apparently breaks the Segger RTT stuff in the SDK
I had the same bug with SEGGER v6.20. What worked for me was to change SEGGER_RTT_Syscalls_SES.c to SEGGER_RTT_Syscalls_GCC.c (for example via the .emProject file).
Thanks for your response @lucas , unfortunately this file does not exist in the Software and API Guide I downloaded. ( DW3000_API_C0_rev4p0 ). Is this perhaps in an older version?
Disabling (removing) the Build for the file SEGGER_RTT_Syscalls_SES.c in the Project works for me.
The project builds without errors then. I did not yet check, which consequences this might have.