DWM3000EVB + ESP32: Inaccurate SS-TWR Distance Readings — Is Centimeter Accuracy Achievable?

  • Qorvo DWM3000EVB (Digi-Key: 2312-DWM3000EVB-ND), qty 2
  • Host MCU: ESP32 DevKitC x2, powered via USB (3.3V logic)
  • Connection: GPIO jumper wires (not stacked shield) — RST=27, IRQ=34, SS=4

FIRMWARE

  • Ranging mode: Single-Sided Two-Way Ranging (SS-TWR)
  • Channel: 5 (6.5 GHz), Preamble: DWT_PLEN_128, PAC: DWT_PAC8, Preamble code: 9
  • Data rate: DWT_BR_6M8, SFD: non-standard, STS: disabled
  • Antenna delay: TX=16385, RX=16385 (both boards, uncalibrated default)
  • Initiator: poll-TX to resp-RX delay = 240 us, RX timeout = 400 us
  • Responder: poll-RX to resp-TX delay = 650 us
  • Post-processing: two-point linear calibration (raw - 0.0622) / 0.8078, 7-sample median filter

FULL CODE

— INITIATOR —

#include “dw3000.h”

#define APP_NAME “SS TWR INIT v1.0”
#define SERIAL_BAUD 115200

const uint8_t PIN_RST = 27;
const uint8_t PIN_IRQ = 34;
const uint8_t PIN_SS = 4;

static dwt_config_t config = {
5,               /\* Channel number. */
DWT_PLEN_128,    /* Preamble length. Used in TX only. */
DWT_PAC8,        /* Preamble acquisition chunk size. Used in RX only. */
9,               /* TX preamble code. Used in TX only. */
9,               /* RX preamble code. Used in RX only. */
1,               /* 0 to use standard 8 symbol SFD, 1 = non-standard 8 symbol */
DWT_BR_6M8,      /* Data rate. */
DWT_PHRMODE_STD, /* PHY header mode. */
DWT_PHRRATE_STD, /* PHY header rate. */
(129 + 8 - 8),   /* SFD timeout \*/
DWT_STS_MODE_OFF,
DWT_STS_LEN_64,
DWT_PDOA_M0
};

#define RNG_DELAY_MS 1000
#define TX_ANT_DLY 16385
#define RX_ANT_DLY 16385

static uint8_t tx_poll_msg[ ] = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0xE0, 0, 0};
static uint8_t rx_resp_msg[ ] = {0x41, 0x88, 0, 0xCA, 0xDE, ‘V’, ‘E’, ‘W’, ‘A’, 0xE1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};

#define ALL_MSG_COMMON_LEN 10
#define ALL_MSG_SN_IDX 2
#define RESP_MSG_POLL_RX_TS_IDX 10
#define RESP_MSG_RESP_TX_TS_IDX 14
#define RESP_MSG_TS_LEN 4

static uint8_t frame_seq_nb = 0;
#define RX_BUF_LEN 20
static uint8_t rx_buffer\[RX_BUF_LEN\];
static uint32_t status_reg = 0;

#define POLL_TX_TO_RESP_RX_DLY_UUS 240
#define RESP_RX_TIMEOUT_UUS 400

static double tof;
static double distance;

static unsigned long success_count = 0;
static unsigned long timeout_count = 0;
static unsigned long error_count = 0;

extern dwt_txconfig_t txconfig_options;

void setup() {
Serial.begin(SERIAL_BAUD);
while (!Serial) { delay(10); }
delay(1000);


spiBegin(PIN_IRQ, PIN_RST);
spiSelect(PIN_SS);
delay(2);

while (!dwt_checkidlerc()) {
    Serial.println("IDLE FAILED");
    while (1);
}

if (dwt_initialise(DWT_DW_INIT) == DWT_ERROR) {
    Serial.println("INIT FAILED");
    while (1);
}

dwt_setleds(DWT_LEDS_ENABLE | DWT_LEDS_INIT_BLINK);

if (dwt_configure(&config)) {
    Serial.println("CONFIG FAILED");
    while (1);
}

dwt_configuretxrf(&txconfig_options);
dwt_setrxantennadelay(RX_ANT_DLY);
dwt_settxantennadelay(TX_ANT_DLY);
dwt_setrxaftertxdelay(POLL_TX_TO_RESP_RX_DLY_UUS);
dwt_setrxtimeout(RESP_RX_TIMEOUT_UUS);
dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE);
}

void loop() {
tx_poll_msg\[ALL_MSG_SN_IDX\] = frame_seq_nb;
dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_TXFRS_BIT_MASK);
dwt_writetxdata(sizeof(tx_poll_msg), tx_poll_msg, 0);
dwt_writetxfctrl(sizeof(tx_poll_msg), 0, 1);
dwt_starttx(DWT_START_TX_IMMEDIATE | DWT_RESPONSE_EXPECTED);

while (!((status_reg = dwt_read32bitreg(SYS_STATUS_ID)) &
         (SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR)));

frame_seq_nb++;

if (status_reg & SYS_STATUS_RXFCG_BIT_MASK) {
    dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK);

    uint32_t frame_len = dwt_read32bitreg(RX_FINFO_ID) & RXFLEN_MASK;
    if (frame_len <= sizeof(rx_buffer)) {
        dwt_readrxdata(rx_buffer, frame_len, 0);

        rx_buffer[ALL_MSG_SN_IDX] = 0;
        if (memcmp(rx_buffer, rx_resp_msg, ALL_MSG_COMMON_LEN) == 0) {

            uint32_t poll_tx_ts, resp_rx_ts, poll_rx_ts, resp_tx_ts;
            int32_t rtd_init, rtd_resp;
            float clockOffsetRatio;

            // 32-bit local timestamps
            poll_tx_ts = dwt_readtxtimestamplo32();
            resp_rx_ts = dwt_readrxtimestamplo32();
            clockOffsetRatio = ((float)dwt_readclockoffset()) / (uint32_t)(1 << 26);

            // Remote timestamps from response payload (also 32-bit, via resp_msg_get_ts)
            resp_msg_get_ts(&rx_buffer[RESP_MSG_POLL_RX_TS_IDX], &poll_rx_ts);
            resp_msg_get_ts(&rx_buffer[RESP_MSG_RESP_TX_TS_IDX], &resp_tx_ts);

            rtd_init = resp_rx_ts - poll_tx_ts;
            rtd_resp = resp_tx_ts - poll_rx_ts;

            tof = ((rtd_init - rtd_resp * (1 - clockOffsetRatio)) / 2.0) * DWT_TIME_UNITS;
            distance = tof * SPEED_OF_LIGHT;

            Serial.print("DISTANCE: ");
            Serial.print(distance, 2);
            Serial.println(" m");

            success_count++;
        }
    }
} else {
    dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR);
    if (status_reg & SYS_STATUS_ALL_RX_TO) timeout_count++;
    if (status_reg & SYS_STATUS_ALL_RX_ERR) error_count++;
}

delay(RNG_DELAY_MS);
}

— RESPONDER —

#include “dw3000.h”

#define APP_NAME “SS TWR RESP v1.0”
#define SERIAL_BAUD 115200

const uint8_t PIN_RST = 27;
const uint8_t PIN_IRQ = 34;
const uint8_t PIN_SS  = 4;

static dwt_config_t config = {
5,
DWT_PLEN_128,
DWT_PAC8,
9,
9,
1,
DWT_BR_6M8,
DWT_PHRMODE_STD,
DWT_PHRRATE_STD,
(129 + 8 - 8),
DWT_STS_MODE_OFF,
DWT_STS_LEN_64,
DWT_PDOA_M0
};

#define TX_ANT_DLY 16385
#define RX_ANT_DLY 16385

// Note: responder reply delay is 650 us; initiator RX window closes at 240+400=640 us
#define POLL_RX_TO_RESP_TX_DLY_UUS 650

static uint8_t rx_poll_msg[ ] = {0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0xE0, 0, 0};
static uint8_t tx_resp_msg[ ] = {0x41, 0x88, 0, 0xCA, 0xDE, ‘V’, ‘E’, ‘W’, ‘A’, 0xE1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};

#define ALL_MSG_COMMON_LEN      10
#define ALL_MSG_SN_IDX          2
#define RESP_MSG_POLL_RX_TS_IDX 10
#define RESP_MSG_RESP_TX_TS_IDX 14
#define RESP_MSG_TS_LEN         4

static uint8_t  frame_seq_nb = 0;
#define RX_BUF_LEN 12
static uint8_t  rx_buffer\[RX_BUF_LEN\];
static uint32_t status_reg = 0;

static uint64_t poll_rx_ts;
static uint64_t resp_tx_ts;

extern dwt_txconfig_t txconfig_options;

void setup() {
Serial.begin(SERIAL_BAUD);
while (!Serial) { delay(10); }
delay(1000);

spiBegin(PIN_IRQ, PIN_RST);
spiSelect(PIN_SS);
delay(2);

while (!dwt_checkidlerc()) {
    Serial.println("IDLE FAILED");
    while (1);
}

if (dwt_initialise(DWT_DW_INIT) == DWT_ERROR) {
    Serial.println("INIT FAILED");
    while (1);
}

dwt_setleds(DWT_LEDS_ENABLE | DWT_LEDS_INIT_BLINK);

if (dwt_configure(&config)) {
    Serial.println("CONFIG FAILED");
    while (1);
}

dwt_configuretxrf(&txconfig_options);
dwt_setrxantennadelay(RX_ANT_DLY);
dwt_settxantennadelay(TX_ANT_DLY);
dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE);

}

void loop() {
dwt_write32bitreg(SYS_STATUS_ID,
SYS_STATUS_RXFCG_BIT_MASK |
SYS_STATUS_ALL_RX_TO       |
SYS_STATUS_ALL_RX_ERR);


dwt_rxenable(DWT_START_RX_IMMEDIATE);

while (!((status_reg = dwt_read32bitreg(SYS_STATUS_ID)) &
         (SYS_STATUS_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR)));

if (status_reg & SYS_STATUS_RXFCG_BIT_MASK) {
    dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_RXFCG_BIT_MASK);

    uint32_t frame_len = dwt_read32bitreg(RX_FINFO_ID) & RXFLEN_MASK;
    if (frame_len <= sizeof(rx_buffer)) {
        dwt_readrxdata(rx_buffer, frame_len, 0);

        rx_buffer[ALL_MSG_SN_IDX] = 0;
        if (memcmp(rx_buffer, rx_poll_msg, ALL_MSG_COMMON_LEN) == 0) {

            // TIME CRITICAL SECTION — no Serial prints until after dwt_starttx()
            poll_rx_ts = get_rx_timestamp_u64();

            uint32_t resp_tx_time =
                (poll_rx_ts + (POLL_RX_TO_RESP_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8;

            dwt_setdelayedtrxtime(resp_tx_time);

            // Predicted TX timestamp written into payload
            resp_tx_ts = (((uint64_t)(resp_tx_time & 0xFFFFFFFEUL)) << 8) + TX_ANT_DLY;

            resp_msg_set_ts(&tx_resp_msg[RESP_MSG_POLL_RX_TS_IDX], poll_rx_ts);
            resp_msg_set_ts(&tx_resp_msg[RESP_MSG_RESP_TX_TS_IDX], resp_tx_ts);

            tx_resp_msg[ALL_MSG_SN_IDX] = frame_seq_nb;
            frame_seq_nb++;

            dwt_writetxdata(sizeof(tx_resp_msg), tx_resp_msg, 0);
            dwt_writetxfctrl(sizeof(tx_resp_msg), 0, 1);
            int tx_result = dwt_starttx(DWT_START_TX_DELAYED);
            // END TIME CRITICAL SECTION

            if (tx_result == DWT_SUCCESS) {
                while (!(dwt_read32bitreg(SYS_STATUS_ID) & SYS_STATUS_TXFRS_BIT_MASK));
                dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_TXFRS_BIT_MASK);
                Serial.println("Response sent OK");
            } else {
                Serial.println("ERROR: Delayed TX failed (too late)");
                dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR);
            }
        }
    }
} else {
    dwt_write32bitreg(SYS_STATUS_ID, SYS_STATUS_ALL_RX_TO | SYS_STATUS_ALL_RX_ERR);
}
}

PROBLEM

We are getting inaccurate and highly variable readings both indoors and outdoors. After applying a two-point linear calibration and a 7-sample median filter, accuracy is still poor — especially at close range and beyond ~5 m.

Raw (uncalibrated) measurements at known distances, boards stationary, face-to-face:

Actual    Low      Mid      High     Spread
0 cm      0.43 m   0.45 m   0.47 m   0.04 m
10 cm    -0.05 m   0.10 m   0.24 m   0.29 m
1 m       0.80 m   0.87 m   0.89 m   0.09 m
10 m      7.53 m   8.14 m   8.76 m   1.23 m

Key observations:

  • At 10 cm, readings are completely unreliable (-0.05 m to +0.24 m, a 0.29 m spread)
  • At 1 m, spread is ~9 cm even after filtering
  • At 10 m indoors, spread reaches 1.23 m
  • Behavior is similar indoors and outdoors, so multipath alone does not seem to be the cause
  • Increasing the median filter from 7 to 32 samples produced no meaningful improvement,
    suggesting the underlying measurements themselves are noisy rather than occasional outlier spikes

WHAT WE HAVE TRIED

  • Verified SPI — dwt_readdevid() returns 0xDECA0302 on both boards
  • Two-point linear calibration from 1 m and 10 m reference points
  • 7-sample and 32-sample median filter — no meaningful difference in accuracy or spread
  • Tested indoors and outdoors — similarly variable in both environments
  • Varied antenna orientation (face-to-face, side-by-side, angled) — no consistent improvement
  • Increased responder reply delay to 650 us to reduce delayed TX failures
  • Enabled LNA/PA on both boards via dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE)

QUESTIONS

  1. TIMING WINDOW MISMATCH
    The initiator opens its RX window 240 us after sending the poll and keeps it open for
    400 us, so the window closes at 640 us. The responder is set to reply at 650 us — 10 us
    after the initiator’s window has already closed. Is this the cause of most of our failed
    or noisy exchanges? What is the correct relationship between POLL_TX_TO_RESP_RX_DLY_UUS,
    RESP_RX_TIMEOUT_UUS, and POLL_RX_TO_RESP_TX_DLY_UUS?
  2. TIMESTAMP ASYMMETRY
    The initiator reads timestamps with dwt_readtxtimestamplo32() and dwt_readrxtimestamplo32()
    (32-bit lower half of the 40-bit counter). The responder reads with get_rx_timestamp_u64()
    (full 64-bit). The original Qorvo example note says 32-bit is safe because the round trip
    is always under 2^32 device time units (~67 ms). But the remote timestamps embedded in the
    response payload are written by resp_msg_set_ts() from the full 64-bit value and then read
    back by resp_msg_get_ts() into a 32-bit variable on the initiator side — could truncation
    there be causing ranging error? Or is the mixed 32/64-bit usage across the two devices
    introducing a subtler inconsistency?
  3. ANTENNA DELAY CALIBRATION
    We are using TX=RX=16385 which is the uncalibrated default. The 0 cm reading of ~0.45 m
    confirms a significant fixed offset. Is there a Qorvo-recommended two-point calibration
    procedure for DWM3000EVB, or a published/community-confirmed starting value for channel 5
    / 6.8 Mbps / preamble code 9?
  4. SS-TWR ACCURACY CEILING
    Once timing and timestamp issues are resolved, is SS-TWR with clock-offset correction
    realistically capable of ~10 cm accuracy at 1-10 m on DW3000, or is DS-TWR required to
    get there? The spread we are seeing persists even with a 32-sample filter, which suggests
    something more fundamental than multipath or occasional outliers.

In short, is it possible to achieve centimeter accuracy for the distance between two DWM3000EVB + ESP32 using the setup that we have here or is it impractical to get our readings down to the nearest centimeter?

Any guidance is greatly appreciated. Thank you!

At very close ranges, the RF signal is so strong that it will saturate the front end and cause poor measurements. 10 cm is not a realistic measurement distance.

Typical readings are about 3 cm std dev, and 9 cm min to max is doing a reasonable job for single measurements.

That feels like multipath despite what you say. Probably bouncing off the ground. Or the range of those modules is at the fringe.

If the 1 m distance is stable within 9 cm, then you don’t have any clock or code issues (those would not be signal strength sensitive). That leaves environmental effects on the RF.

Both indoor and outdoor have a ground/floor to bounce off of.

I don’t believe the DWM3000 has either an LNA or PA. it is not evident in the block diagram in the DS:

Calibrating antenna delay is a bit tricky since it is slightly signal strength dependent.

My suggestion would be to place the units a known distance apart in the middle of your desired measurement range (half way to max range, say). Then adjust antenna delay until it averages the actual distance. You will find there is some non linearity in it due to signal strength effects.

Also, the orientation of the antenna can make a big difference as this affects not only signal strength but also group delay. You will have to pick an antenna delay that overall minimizes the error over distance and orientations, but there is no perfect value.

That’s a good question that I don’t know the answer to. My impression is that DS-TWR is noticeably more accurate than SS-TWR. Is DS-TWR not an option? What drives you to use SS-TWR?

For defined antenna orientations, you can calibrate the true distance versus measured distance over the range of measurement, plus averaging samples, you should get to 1 cm accuracy, but it isn’t easy. If you have to deal with antenna orientations changing, you likely can’t get to 1 cm accuracy.

Getting 1 cm precision (repeatability) would be relatively easy, however.


Mike Ciholas, President, Ciholas, Inc
3700 Bell Road, Newburgh, IN 47630 USA
mikec@ciholas.com

Hello Mike,
Just to clarify on some of your answers, you said 10 cm is not a realistic measurement distance but it’s possible to get 1 cm accuracy; do you mean that distances at like 1 meter it’s possible to get 1 cm accuracy but anything lower than that it’s not realistic? Could you also explain how to get 1cm precision readings? How the antennas are oriented; is it okay if the antennas are pointed up but they can rotate? We weren’t aware if DS-TWR was an option for the DWM3000 so that’s why we didn’t consider it.

Best,
Sivaram Saravanakumaran, Software Engineer, Mobile Entertainment, LLC
sivaram.saravanakumaran@humanonastick.com

Correct. It is too close, the RF signal too strong, to get accurate results.

I suppose it is possible you can make a system which dynamically reduces transmit power as it gets closer to avoid this problem, but even so, 10 cm is very close.

There is some distance where the inaccuracy starts to get problematic. This will depend on signal power, antennas, orientation, LNA equipped or not, unit to unit variation, etc. So the exact distance at which this occurs is variable and somewhat subjective as to your accuracy criteria.

1 cm precision is easy, simply average a lot of readings.

1 cm accuracy is harder since various inaccuracies always exist in the system such as antenna delay calibration, unit to unit variation, etc. To achieve 1 cm accuracy with an UWB system requires great effort. My post indicated that you would need controlled antenna orientations and to build a measured versus real distance conversion chart to correct for deviations. Whether these constraints work for your application is not known to me since I don’t know what you are really trying to do. It is hard to give useful advice not knowing your application.

You will find that rotating antennas causing some distance variations. This is because the group delay of the antenna varies with reception direction.

Since we built our own UWB code base, I am not that familiar with what options you have available. That being said, I thought DS-TWR was a common operating mode that dates way back to the first UWB chips, so I would be surprised if it isn’t a choice.


Mike Ciholas, President, Ciholas, Inc
3700 Bell Road, Newburgh, IN 47630 USA
mikec@ciholas.com

Hello Mike,

Thank you for clarifying the questions I asked. To give you a bit of context on the application I’m working on, we are a Segway-based touring company in Minnesota that provides history tours in Minneapolis and St. Paul. We were planning on using the Qorvo UWBs and ESP32, that are attached to a Segway, to see if we could get accurate location and distance between multiple Segways (up to 80) during a tour. Is this plan feasible? I was also wondering how the antennas should be oriented to reduce distance error? If the antennas are always pointed straight up but the Segways move/rotate around, would this mess up the ranging and cause distance variations?

Best,
Sivaram Saravanakumaran, Software Engineer, Mobile Entertainment, LLC
sivaram.saravanakumaran@humanonastick.com

Hi Sivaram,

I understand the core of the issues is that you are unable to use standard libraries because of esp32, which is not ARM Cortex-M4/M33 core. So you cannot run or port standard uwbstack libraries with FiRa based TWR to esp32. That’s the issue… sorry cannot help.

For SS-TWR its performance is fundamentally affected by CFO estimations on the receiver sides. To cancel the effect of CFO please use DS-TWR…

What do you mean exactly by “location”?

It sounds like you want to display the relative map of multiple mobile objects using UWB, perhaps relative to a lead unit.

In theory, if you had the range between all units, you could take that data and crunch it through an algorithm to find the relative location of all the units. This presumes you avoid certain weird edge cases, like N-1 units are in a straight line leaving the last unit offset to the line, but you don’t know which direction that offset is. With a more random dispersion, it should be possible mathematically.

If you have 80 units, there are 3160 possible range pairs, which is an exceedingly large number. It takes time to transmit from each unit, and then it becomes difficult to send out your answers since that would take kilobytes of messages for each unit.

This means you have to develop a methodology that is sparse on range pairs, but yet gets you enough data to resolve the information you want. This will be challenging since you don’t have any control over the formation as it moves, so knowing which range pairs to use is not obvious, and it has to be a stable distributed algorithm.

Not clearly so as stated. Maybe I have misunderstood the details. There is not enough air time to realistically get all the range pairs. SS-TWR does use 2 packets versus 3 for DS-TWR, so that is one reason to consider it, but even that won’t solve this case.

The problem as stated also has no central control, so the system has to work without a central coordinating resource.

One possible concept: a lead unit has an AOA phased array system and it does SS-TWR with each of the follower units. This would then allow the lead unit to build a map of the followers. None of the followers would have this map (unless sent to them separately). The lead unit could have something like our phased array 360 degree AOA unit shown here:

In this setup, you have a central resource to coordinate things and only 79 interaction to maps the fleet of 80 units, which is quite doable up to, maybe 10 Hz update rate.

The video above is quite old and we never commercialized the anchor, so it would take some development to make usable unit in the field. It an be made smaller at the expense of angular accuracy. Only the lead unit needs the array, all other units can be simple tags.

Are you generally outdoors with moderately decent sky visibility? Might consider GPS or even RTK GPS. That will not only give you relative position, but also absolute position. This won’t work if you go into buildings, in tunnels, under overpasses, or are surrounded by skyscrapers (the urban canyon problem).

A vertically polarized antenna on each unit would work well. You will get body and machine occlusion as the machine rotates, but that’s not an antenna issue, but a signal blockage.

Since Segway riders wear a helmet, putting a tag on the helmet results in less obstructions and likely better results.

If you could compute the formation layout, what are you doing with that information? Is it being displayed to a leader? Logged for analytics? Used to detect stragglers or lost units? It is hard to suggest an improved concept without knowing the high level objective.


Mike Ciholas, President, Ciholas, Inc
3700 Bell Road, Newburgh, IN 47630 USA
mikec@ciholas.com

Reading the problem description a GPS and short range radio seems like the logical solution. Each unit simply broadcasts its location. The guide can then pick these up and display on a map where they are and where everyone is relative to them. I’m assuming the aim is to check someone doesn’t wander off rather than warn if they are about to collide with cm accuracy. Unless you’re indoors or in a tunnel just about any modern GNSS should be good enough accuracy to get you to within 1-2 Segway widths of correct.
Or replace the short range radio with a cellular modem, cost / running cost goes up a bit but a central office can then track every unit remotely no matter where they are. That would also have potential anti-theft advantages. That sort of system is available off the shelf.

UWB is a great solution for some situations but this doesn’t sound like one of them.

Hi, I was able to get down to about 35cm and that was with about 2-4cm accuracy, after that near-field kicks in, antenna radiation pattern is not ideal and the first-path detection becomes less perfect. At 1m and above its quite stable.