Hello, I am currently working with DWM3000 and I am trying to test the different modes of operation. When in RX, the module retrieves the frames as expected and I can extract the timestamps, which look fine to me, as they increment on a similar scale (the TX is transmitted periodically). On the other side though, the TX has some issues. The frame is sent correctly, no issues there, but when trying to read the TX timestamp (via dwm_readtxtimestamp()), the first byte in the timestamp buffer seem to always be 0x01, no matter how long I keep the TX on. Note that I tried implementing this both with polling and with callbacks, both throwing the same issues. Might there be configuration issues? Has anyone encountered a similar problem?
-
example RX buffers (base 10):
rx: 217 121 203 123 059
rx: 228 169 032 073 074
rx: 195 069 022 041 089
rx: 166 216 166 009 104 -
example TX buffers (base 10):
tx: 001 038 049 125 059
tx: 001 158 094 235 118
tx: 001 206 202 219 099
Note that the first byte always stays 0x01.
Edit: after trying reading directly from the register address (bypassing the API), I can confirm that the value of the byte never changes.