Hi, I am the embedded/IoT beginner using Beagleboard ai 64.
I was wondering is there any way to get raw data from dwm1000/dwm3000 with using adaptor board only? I used arduino board at the beginning and it worked, but since arduino is not suitable for my project, changed it to the Beagleboard which is similar to Raspberry Pi I guess.
On the adaptor board, I could see IRQ/MISO/MOSI/RST are needed for run.
- I thought spidev_test.c would receive data from the UWB module.
But the result is 00 00 00 00 00 00 …
(I checked loopback test working well)
what did I miss? How should I assign IRQ/RST pin to embedded board?
p.s. if mcu board needed to run DWM3000 board, I am considering buying DWM3001C. Without development kit, how do I flash and upload code through the board? through UART?