Hi,
I recently received a set of DWS3000 Arduino shields. I am using them together with the STM Nucleo F429ZI. The normal setup and the examples do work fine, but I managed to change some TX settings that started some RX errors on the other side.
I wanted to further understand how those errors might occur, but I could not find any explanations for the different error codes in the status register. I checked with the SYS_STATUS_ALL_RX_ERR and realized that the Bit mask SYS_STATUS_RXSTO_BIT_MASK matches my error.
Is there any documentation available what those errors actually mean? I could not find them in the documentation pdfs or the source code. Any help is appreciated. Thank you.
Kind regards
Alexander
AndyA
May 27, 2021, 1:39pm
2
Going by this post from last week the user manual for the DW3000 should be out very soon. That should give definitions for all of the status register bits.
Alex-1
June 16, 2021, 10:13am
4
I have not seen any updates on this.
One thing that I managed to understand is that most system status codes are copied from the DW1000 codes and there they have been documented. So here’s a list of RX related status codes that where I copied the meaning from the DW1000:
#define SYS_STATUS_ID 0x44
#define SYS_STATUS_LEN (4U)
#define SYS_STATUS_MASK 0xFFFFFFFFUL
#define SYS_STATUS_ARFE_BIT_OFFSET (29U)
#define SYS_STATUS_ARFE_BIT_LEN (1U)
#define SYS_STATUS_ARFE_BIT_MASK 0x20000000UL /* Automatic Frame Filtering rejection */
#define SYS_STATUS_CPERR_BIT_OFFSET (28U)
#define SYS_STATUS_CPERR_BIT_LEN (1U)
#define SYS_STATUS_CPERR_BIT_MASK 0x10000000UL /* COULD BE: Mask Transmit Buffer Error event */
#define SYS_STATUS_HPDWARN_BIT_OFFSET (27U)
#define SYS_STATUS_HPDWARN_BIT_LEN (1U)
#define SYS_STATUS_HPDWARN_BIT_MASK 0x8000000UL /* Mask Half Period Delay Warning event */
#define SYS_STATUS_RXSTO_BIT_OFFSET (26U)
#define SYS_STATUS_RXSTO_BIT_LEN (1U)
#define SYS_STATUS_RXSTO_BIT_MASK 0x4000000UL /* Mask Receive SFD timeout event */
#define SYS_STATUS_PLL_HILO_BIT_OFFSET (25U)
#define SYS_STATUS_PLL_HILO_BIT_LEN (1U)
#define SYS_STATUS_PLL_HILO_BIT_MASK 0x2000000UL /* Mask Clock PLL Loosing Lock warning event */
#define SYS_STATUS_RCINIT_BIT_OFFSET (24U)
#define SYS_STATUS_RCINIT_BIT_LEN (1U)
#define SYS_STATUS_RCINIT_BIT_MASK 0x1000000UL /*COULD BE: RF PLL Losing Lock */
#define SYS_STATUS_SPIRDY_BIT_OFFSET (23U)
#define SYS_STATUS_SPIRDY_BIT_LEN (1U)
#define SYS_STATUS_SPIRDY_BIT_MASK 0x800000UL /*COULD BE: SLEEP to INIT */
#define SYS_STATUS_RXPTO_BIT_OFFSET (21U)
#define SYS_STATUS_RXPTO_BIT_LEN (1U)
#define SYS_STATUS_RXPTO_BIT_MASK 0x200000UL /* Preamble detection timeout */
#define SYS_STATUS_RXOVRR_BIT_OFFSET (20U)
#define SYS_STATUS_RXOVRR_BIT_LEN (1U)
#define SYS_STATUS_RXOVRR_BIT_MASK 0x100000UL /* Receiver Overrun */
#define SYS_STATUS_VWARN_BIT_OFFSET (19U)
#define SYS_STATUS_VWARN_BIT_LEN (1U)
#define SYS_STATUS_VWARN_BIT_MASK 0x80000UL /* ??? */
#define SYS_STATUS_CIAERR_BIT_OFFSET (18U)
#define SYS_STATUS_CIAERR_BIT_LEN (1U)
#define SYS_STATUS_CIAERR_BIT_MASK 0x40000UL /* COULD BE: Mask leading edge detection processing error event */
#define SYS_STATUS_RXFTO_BIT_OFFSET (17U)
#define SYS_STATUS_RXFTO_BIT_LEN (1U)
#define SYS_STATUS_RXFTO_BIT_MASK 0x20000UL /* Mask Receive Frame Wait Timeout event */
#define SYS_STATUS_RXFSL_BIT_OFFSET (16U)
#define SYS_STATUS_RXFSL_BIT_LEN (1U)
#define SYS_STATUS_RXFSL_BIT_MASK 0x10000UL /* Mask receiver Reed Solomon Frame Sync Loss event */
#define SYS_STATUS_RXFCE_BIT_OFFSET (15U)
#define SYS_STATUS_RXFCE_BIT_LEN (1U)
#define SYS_STATUS_RXFCE_BIT_MASK 0x8000U /* Receiver FCS (Frame Check Sequence) Error */
#define SYS_STATUS_RXFCG_BIT_OFFSET (14U)
#define SYS_STATUS_RXFCG_BIT_LEN (1U)
#define SYS_STATUS_RXFCG_BIT_MASK 0x4000U /* Receiver FCS (Frame Check Sequence) Good */
#define SYS_STATUS_RXFR_BIT_OFFSET (13U)
#define SYS_STATUS_RXFR_BIT_LEN (1U)
#define SYS_STATUS_RXFR_BIT_MASK 0x2000U /* Mask receiver data frame ready event */
#define SYS_STATUS_RXPHE_BIT_OFFSET (12U)
#define SYS_STATUS_RXPHE_BIT_LEN (1U)
#define SYS_STATUS_RXPHE_BIT_MASK 0x1000U /* Mask receiver PHY header error event */
#define SYS_STATUS_RXPHD_BIT_OFFSET (11U)
#define SYS_STATUS_RXPHD_BIT_LEN (1U)
#define SYS_STATUS_RXPHD_BIT_MASK 0x800U /* Mask receiver PHY header detect event */
#define SYS_STATUS_CIADONE_BIT_OFFSET (10U)
#define SYS_STATUS_CIADONE_BIT_LEN (1U)
#define SYS_STATUS_CIADONE_BIT_MASK 0x400U /*Could be: Mask LDE (leading edge detection) processing done event */
#define SYS_STATUS_RXSFDD_BIT_OFFSET (9U)
#define SYS_STATUS_RXSFDD_BIT_LEN (1U)
#define SYS_STATUS_RXSFDD_BIT_MASK 0x200U /* Mask receiver SFD detected event */
#define SYS_STATUS_RXPRD_BIT_OFFSET (8U)
#define SYS_STATUS_RXPRD_BIT_LEN (1U)
#define SYS_STATUS_RXPRD_BIT_MASK 0x100U /* Mask receiver preamble detected event */
AndyA
June 16, 2021, 1:09pm
5
The DW3000 user manual came out over two weeks ago. It’s available from https://www.decawave.com/wp-content/uploads/2021/05/DW3000-User-Manual-1.pdf
Section 8.2.2.14, page 90 onwards, gives details of the status register.
Alex-1
June 16, 2021, 2:04pm
6
Ah that’s great. Where did you find it? It was not listed at the product pages DWM3000 Module - Decawave
nor on Qorvo site for the DW3000 products
Alex-1
June 16, 2021, 2:18pm
7
It’s listed at Design Center → DW3000IC (but only there)