Hello I’m making a setup of a TDoA RTLS Systems, we are using the DWM1004 Module for tags with the latest version of the TDOA Firmware for DWM1004C, the problem that we have is that is not possible to set a different channel of 2 or 5, we want to use the channel 1, we get the legend “error function” when we try to set it:
- Is this a bug or a restriction for some reason?
- There is any way to solve it easily?
*I understand the antenna of the DWM1004C is capable to cover the full bandwidth range of DW UWB, there is needed to calibrate something in the OTP Memory for the channels 1 3 4 6?
*See attached picture of the a terminal app trying to set different cannels in the DWM1004C
JS0091{“Info”:{
“Device”:“DWM1004C TDoA Tag”,
“Version”:“5.1.0”,
“Build”:“Dec 19 2019 15:05:35”,
“Driver”:“DW1000 Device Driver Version 05.01.01”}}
JS00E9{“UWB PARAM”:{
“CHAN”:5,
“PRF”:64,
“PLEN”:128,
“DATARATE”:6810,
“TXCODE”:11,
“PAC”:8,
“NSSFD”:0,
“PHRMODE”:0,
“SMARTPOWER”:1,
“BLINKFAST”:100,
“BLINKSLOW”:100,
“RANDOMNESS”:10,
“TAGIDSET”:0,
“TAGID”:0xdeca010048f154af}}
Best regards.