I have a few dwm1004 with the dev board that are not in use, can i flash the dwm1001 firmware into it to work as a 1001 tag? or it is not compatible? Thanks
Hi Thiago,
The firmware for DWM1001 is not compatible with DWM1004.
A TDoA Tag application for DWM1004 is available on Decawave’s website.
Hope it helps,
Yves
Oh, ok. Thank you.
By that you mean a possibility of real world application or a software? Could you point me where?
Have a look at the resource package there :
Note this is only TDoA Tag application, so if you don’t have a TDoA network (with anchors), you can’t do much with it. If you’re not too familiar with TDoA maybe have a look on the forum and on the web, there are multiples subjets/documents explaining it in detail.
Yves