Hi,
I’m communicating with DWM1001C tag node (running PANS firmware) using UART TLV. The command dwm_status_get is sent to get loc_data bit then if this bit is 1, the command dwm_loc_get is sent to get location data. This routine is running with 10 Hz rate.
While running this routine, I notice that sometimes the tag does not response the dwm_status_get command for about 12-14 seconds but after that it comes back to response. Are there any issue with my approach or the module itself and how can I handle this problem correctly.
Thank you