Hardik
September 9, 2020, 12:05pm
1
Dear ,
I bought DWM1001C Module thought that it will be easy to use but I have no idea how to flash firmware into Module.
I am having J-Link (JTAG) and DWM1001C Module.
Can you please help me to understand how we can Flash firmware into Module.
Thanks & Regards,
Hardik
DavidF
September 9, 2020, 2:00pm
2
Hi Hardik,
You will need a J-Link (I use the J-Link EDU), and you will use the SWD interface.
SWDIO / SWDCLK / GND / +5V / VTREF.
And you can use the J-Flash Lite software to flash the PANS R2 in the module.
Hardik
September 10, 2020, 6:00am
3
Thanks DevidF for your Reply.
I am having Same J-Link EDU.
I am giving 3.3 V to Board VCC , Where i need to give 5V because board is supporting 3.6 Max Vlt.
I connect as Shown in Image. Can you please suggest me where i am doing Mistake .
Thanks & Regards,
Hardik
DavidF
September 10, 2020, 6:57am
4
You need to connect the Vref of the J-Link EDU, you must connect the Vref of the J-Link to the VCC of the DWM1001C.
In addition, you can connect the RESET signal from the J-LINK to the DWM1001C.
DavidF
September 10, 2020, 7:34am
6
Great news !
An advice I can give to you, if you create a custom board if the DWM1001C.
Put on the board a connector like this one : https://www.segger.com/products/debug-probes/j-link/accessories/adapters/6-pin-needle-adapter/
It works very well.