This is not supported in the DWM1001 only TWR. We should remove the TypeDef from the header file. Sorry for the confusion.
FYI - We will be soon releasing a Keil MDK projects with ports of some of the basic DWM1000 API examples so maybe with that you can easily port your own TDoA tag code?
Thanks! It was more of a glimmer of hope-- the datasheet made it clear that wasn’t really an option.
I think my plan is to just target the nRF52 directly, since I can’t find API functions to do what I need. I sent an e-mail to sales@ this morning, but since I’m here: is there documentation anywhere about the connections between the nRF52 and the DW1000?
We will not be releasing the schematics for the module.
The information above should suffice. All the other Nordic GPIO’s are brought out on the module as indicated in the Module DS.
Thanks. This are good information.
Can you also provide information for the other pins too.
Thanks.
Decaware DM1000 UWB chip Nordic nRF52832 chip Function
Wakeup (pin 2) <------ ??? This is to wake up the decaware chip
GPIO5/SPIPOL (pin10) <------ ??? This two pins dictate the SPI Mode (0,1,2,3)
GPIO6/SPIPHA (pin 9) <------ ??? Are these pins connects to the processor or
the SPI Mode is default to 0