Hello ,
I am having MDEK 1001 with Raspberry 3 B+ I check all the below things
Raspberry Pi version
-
Which Raspberry hardware revision are you using? If possible please send a picture of the Raspberry with the DWM1001.
Raspberry pi 3 B+ ( Linux raspberrypi 4.14.50-v7+ #1122 SMP Tue Jun 19 12:26:26 BST 2018 armv7l GNU/Linux)
-
Is the DWM1001 reflashed with the R2 binary?
I am using MDEK 1001 new device -
Which Raspberry Image are you using? The official one from the Release 2?
Official one DRTLS_raspbian_R2.0.img -
How do you start the DWM Daemon? Manually or just restarted the Raspberry?
Just restarted the Raspberry -
Can you get the system working or it keeps failing like this?
it keep failing like this -
Can you enter the module shell using: minicom -D /dev/serial0 (and double enter)?
yes
-
Please send outputs of the commands on the failing system:
-
lsmod
pi@raspberrypi:~ $ lsmod
Module Size Used by
rfcomm 49152 6
cmac 16384 1
bnep 20480 2
hci_uart 36864 1
btbcm 16384 1 hci_uart
serdev 20480 1 hci_uart
bluetooth 368640 29 hci_uart,bnep,btbcm,rfcomm
ecdh_generic 28672 1 bluetooth
fuse 106496 3
spidev 16384 0
brcmfmac 307200 0
brcmutil 16384 1 brcmfmac
cfg80211 573440 1 brcmfmac
rfkill 28672 6 bluetooth,cfg80211
snd_bcm2835 32768 1
snd_pcm 98304 1 snd_bcm2835
snd_timer 32768 1 snd_pcm
snd 69632 5 snd_timer,snd_bcm2835,snd_pcm
spi_bcm2835 16384 0
uio_pdrv_genirq 16384 0
uio 20480 1 uio_pdrv_genirq
fixed 16384 0
dwm 77824 4
i2c_dev 16384 0
ip_tables 24576 0
x_tables 32768 1 ip_tables
ipv6 434176 40 -
ls -la /dev/dwm0
pi@raspberrypi:~ $ ls -la /dev/dwm0
crw------- 1 root root 200, 0 Aug 5 17:52 /dev/dwm0 -
ps ax | grep dwm
pi@raspberrypi:~ $ ps ax | grep dwm
446 ? Sl 0:01 /usr/local/bin/dwm-proxy -c /etc/dwm1001/dwm1001-proxy.config
453 ? Sl 0:00 /usr/local/bin/dwm-daemon -c /etc/dwm1001/dwm1001.config -l /var/log/dwm-daemon.log
2234 pts/0 S+ 0:00 grep --color=auto dwm
I check the pin continuity its fine attached the image for the same .
Please support its urgent . Thank you in advance for your support .
Error Message
Error Msg
pi@raspberrypi:~ $ dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.50-v7+ (dc4@dc4-XPS13-9333) (gcc version 4.9.3 (crosstool-NG crosstool-ng-1.22.0-88-g8460611)) #1122 SMP Tue Jun 19 12:26:26 BST 2018
[ 0.000000] CPU: ARMv7 Processor [410fd034] revision 4 (ARMv7), cr=10c5383d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Raspberry Pi 3 Model B Plus Rev 1.3
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] cma: Reserved 8 MiB at 0x3ac00000
[ 0.000000] On node 0 totalpages: 242688
[ 0.000000] free_area_init_node: node 0, pgdat 80c85000, node_mem_map ba3a1000
[ 0.000000] Normal zone: 2133 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 242688 pages, LIFO batch:31
[ 0.000000] percpu: Embedded 17 pages/cpu @ba34a000 s38720 r8192 d22720 u69632
[ 0.000000] pcpu-alloc: s38720 r8192 d22720 u69632 alloc=17*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 240555
[ 0.000000] Kernel command line: 8250.nr_uarts=1 bcm2708_fb.fbwidth=656 bcm2708_fb.fbheight=416 bcm2708_fb.fbswap=1 vc_mem.mem_base=0x3ec00000 vc_mem.mem_size=0x40000000 dwc_otg.lpm_enable=0 console=tty1 root=PARTUUID=c049f471-02 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait quiet splash plymouth.ignore-serial-consoles
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 940236K/970752K available (7168K kernel code, 575K rwdata, 2072K rodata, 1024K init, 706K bss, 22324K reserved, 8192K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xbb800000 - 0xff800000 (1088 MB)
lowmem : 0x80000000 - 0xbb400000 ( 948 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80800000 (8160 kB)
.init : 0x80b00000 - 0x80c00000 (1024 kB)
.data : 0x80c00000 - 0x80c8fef4 ( 576 kB)
.bss : 0x80c96f40 - 0x80d478b4 ( 707 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] ftrace: allocating 25253 entries in 75 pages
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] arch_timer: cp15 timer(s) running at 19.20MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x46d987e47, max_idle_ns: 440795202767 ns
[ 0.000007] sched_clock: 56 bits at 19MHz, resolution 52ns, wraps every 4398046511078ns
[ 0.000018] Switching to timer-based delay loop, resolution 52ns
[ 0.000263] Console: colour dummy device 80x30
[ 0.000279] console [tty1] enabled
[ 0.000307] Calibrating delay loop (skipped), value calculated using timer frequency… 38.40 BogoMIPS (lpj=192000)
[ 0.000323] pid_max: default: 32768 minimum: 301
[ 0.000642] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000656] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001589] Disabling memory control group subsystem
[ 0.001669] CPU: Testing write buffer coherency: ok
[ 0.002059] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002437] Setting up static identity map for 0x100000 - 0x10003c
[ 0.002553] Hierarchical SRCU implementation.
[ 0.003185] smp: Bringing up secondary CPUs …
[ 0.003867] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.004613] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.005341] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.005445] smp: Brought up 1 node, 4 CPUs
[ 0.005455] SMP: Total of 4 processors activated (153.60 BogoMIPS).
[ 0.005461] CPU: All CPU(s) started in HYP mode.
[ 0.005465] CPU: Virtualization extensions available.
[ 0.006319] devtmpfs: initialized
[ 0.016235] random: get_random_u32 called from bucket_table_alloc+0xfc/0x24c with crng_init=0
[ 0.016966] VFP support v0.3: implementor 41 architecture 3 part 40 variant 3 rev 4
[ 0.017185] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.017203] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.017758] pinctrl core: initialized pinctrl subsystem
[ 0.018494] NET: Registered protocol family 16
[ 0.021178] DMA: preallocated 1024 KiB pool for atomic coherent allocations
[ 0.026012] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.026019] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.026227] Serial: AMBA PL011 UART driver
[ 0.027844] bcm2835-mbox 3f00b880.mailbox: mailbox enabled
[ 0.028299] uart-pl011 3f201000.serial: could not find pctldev for node /soc/gpio@7e200000/uart0_pins, deferring probe
[ 0.059867] bcm2835-dma 3f007000.dma: DMA legacy API manager at bb813000, dmachans=0x1
[ 0.061373] SCSI subsystem initialized
[ 0.061604] usbcore: registered new interface driver usbfs
[ 0.061655] usbcore: registered new interface driver hub
[ 0.061738] usbcore: registered new device driver usb
[ 0.070091] raspberrypi-firmware soc:firmware: Attached to firmware from 2018-06-07 15:31
[ 0.071485] clocksource: Switched to clocksource arch_sys_counter
[ 0.148507] VFS: Disk quotas dquot_6.6.0
[ 0.148591] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.148776] FS-Cache: Loaded
[ 0.148973] CacheFiles: Loaded
[ 0.157747] NET: Registered protocol family 2
[ 0.158467] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.158576] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.158761] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.158891] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.158935] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.159162] NET: Registered protocol family 1
[ 0.159594] RPC: Registered named UNIX socket transport module.
[ 0.159600] RPC: Registered udp transport module.
[ 0.159605] RPC: Registered tcp transport module.
[ 0.159610] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.161124] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 7 counters available
[ 0.163970] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.171910] FS-Cache: Netfs ‘nfs’ registered for caching
[ 0.172501] NFS: Registering the id_resolver key type
[ 0.172534] Key type id_resolver registered
[ 0.172539] Key type id_legacy registered
[ 0.172554] nfs4filelayout_init: NFSv4 File Layout Driver Registering…
[ 0.174417] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 251)
[ 0.174538] io scheduler noop registered
[ 0.174545] io scheduler deadline registered (default)
[ 0.174816] io scheduler cfq registered
[ 0.174823] io scheduler mq-deadline registered
[ 0.174829] io scheduler kyber registered
[ 0.177097] BCM2708FB: allocated DMA memory fad00000
[ 0.177121] BCM2708FB: allocated DMA channel 0 @ bb813000
[ 0.185645] Console: switching to colour frame buffer device 82x26
[ 0.190805] Serial: 8250/16550 driver, 1 ports, IRQ sharing enabled
[ 0.192143] bcm2835-rng 3f104000.rng: hwrng registered
[ 0.192276] vc-mem: phys_addr:0x00000000 mem_base=0x3ec00000 mem_size:0x40000000(1024 MiB)
[ 0.192745] vc-sm: Videocore shared memory driver
[ 0.193019] gpiomem-bcm2835 3f200000.gpiomem: Initialised: Registers at 0x3f200000
[ 0.202506] brd: module loaded
[ 0.211031] loop: module loaded
[ 0.211043] Loading iSCSI transport class v2.0-870.
[ 0.211762] libphy: Fixed MDIO Bus: probed
[ 0.211859] usbcore: registered new interface driver lan78xx
[ 0.211911] usbcore: registered new interface driver smsc95xx
[ 0.211926] dwc_otg: version 3.00a 10-AUG-2012 (platform bus)
[ 0.440041] Core Release: 2.80a
[ 0.440050] Setting default values for core params
[ 0.440082] Finished setting default values for core params
[ 0.640323] Using Buffer DMA mode
[ 0.640330] Periodic Transfer Interrupt Enhancement - disabled
[ 0.640335] Multiprocessor Interrupt Enhancement - disabled
[ 0.640342] OTG VER PARAM: 0, OTG VER FLAG: 0
[ 0.640350] Dedicated Tx FIFOs mode
[ 0.640752] WARN::dwc_otg_hcd_init:1046: FIQ DMA bounce buffers: virt = 0xbad14000 dma = 0xfad14000 len=9024
[ 0.640776] FIQ FSM acceleration enabled for :
Non-periodic Split Transactions
Periodic Split Transactions
High-Speed Isochronous Endpoints
Interrupt/Control Split Transaction hack enabled
[ 0.640783] dwc_otg: Microframe scheduler enabled
[ 0.640829] WARN::hcd_init_fiq:459: FIQ on core 1 at 0x805e7d20
[ 0.640840] WARN::hcd_init_fiq:460: FIQ ASM at 0x805e8088 length 36
[ 0.640852] WARN::hcd_init_fiq:486: MPHI regs_base at 0xbb87e000
[ 0.640903] dwc_otg 3f980000.usb: DWC OTG Controller
[ 0.640934] dwc_otg 3f980000.usb: new USB bus registered, assigned bus number 1
[ 0.640963] dwc_otg 3f980000.usb: irq 62, io mem 0x00000000
[ 0.641009] Init: Port Power? op_state=1
[ 0.641014] Init: Power Port (0)
[ 0.641214] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.641224] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.641232] usb usb1: Product: DWC OTG Controller
[ 0.641240] usb usb1: Manufacturer: Linux 4.14.50-v7+ dwc_otg_hcd
[ 0.641248] usb usb1: SerialNumber: 3f980000.usb
[ 0.641856] hub 1-0:1.0: USB hub found
[ 0.641895] hub 1-0:1.0: 1 port detected
[ 0.642389] dwc_otg: FIQ enabled
[ 0.642394] dwc_otg: NAK holdoff enabled
[ 0.642399] dwc_otg: FIQ split-transaction FSM enabled
[ 0.642409] Module dwc_common_port init
[ 0.642621] usbcore: registered new interface driver usb-storage
[ 0.642784] mousedev: PS/2 mouse device common for all mice
[ 0.642853] IR NEC protocol handler initialized
[ 0.642859] IR RC5(x/sz) protocol handler initialized
[ 0.642864] IR RC6 protocol handler initialized
[ 0.642869] IR JVC protocol handler initialized
[ 0.642874] IR Sony protocol handler initialized
[ 0.642879] IR SANYO protocol handler initialized
[ 0.642884] IR Sharp protocol handler initialized
[ 0.642889] IR MCE Keyboard/mouse protocol handler initialized
[ 0.642894] IR XMP protocol handler initialized
[ 0.643551] bcm2835-wdt 3f100000.watchdog: Broadcom BCM2835 watchdog timer
[ 0.644469] bcm2835-cpufreq: min=600000 max=1400000
[ 0.644812] sdhci: Secure Digital Host Controller Interface driver
[ 0.644817] sdhci: Copyright(c) Pierre Ossman
[ 0.645165] mmc-bcm2835 3f300000.mmc: could not get clk, deferring probe
[ 0.645479] sdhost-bcm2835 3f202000.mmc: could not get clk, deferring probe
[ 0.645573] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.646963] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.647098] hidraw: raw HID events driver (C) Jiri Kosina
[ 0.647262] usbcore: registered new interface driver usbhid
[ 0.647267] usbhid: USB HID core driver
[ 0.647842] vchiq: vchiq_init_state: slot_zero = bad80000, is_master = 0
[ 0.649196] [vc_sm_connected_init]: start
[ 0.657845] [vc_sm_connected_init]: end - returning 0
[ 0.658393] Initializing XFRM netlink socket
[ 0.658414] NET: Registered protocol family 17
[ 0.658502] Key type dns_resolver registered
[ 0.659002] Registering SWP/SWPB emulation handler
[ 0.659545] registered taskstats version 1
[ 0.665428] uart-pl011 3f201000.serial: cts_event_workaround enabled
[ 0.665509] 3f201000.serial: ttyAMA0 at MMIO 0x3f201000 (irq = 87, base_baud = 0) is a PL011 rev2
[ 0.666979] 3f215040.serial: ttyS0 at MMIO 0x0 (irq = 166, base_baud = 31250000) is a 16550
[ 0.667832] mmc-bcm2835 3f300000.mmc: mmc_debug:0 mmc_debug2:0
[ 0.667841] mmc-bcm2835 3f300000.mmc: DMA channel allocated
[ 0.722067] sdhost: log_buf @ bad13000 (fad13000)
[ 0.760774] mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
[ 0.762340] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
[ 0.763889] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
[ 0.766666] mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
[ 0.801502] mmc0: sdhost-bcm2835 loaded - DMA enabled (>1)
[ 0.802506] of_cfs_init
[ 0.802645] of_cfs_init: OK
[ 0.803165] Waiting for root device PARTUUID=c049f471-02…
[ 0.843789] random: fast init done
[ 0.851795] mmc1: new high speed SDIO card at address 0001
[ 0.861664] Indeed it is in host mode hprt0 = 00021501
[ 0.959759] mmc0: host does not support reading read-only switch, assuming write-enable
[ 0.963774] mmc0: new high speed SDHC card at address aaaa
[ 0.964244] mmcblk0: mmc0:aaaa SD32G 29.7 GiB
[ 0.965605] mmcblk0: p1 p2
[ 0.983452] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[ 0.983460] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[ 1.071528] usb 1-1: new high-speed USB device number 2 using dwc_otg
[ 1.071666] Indeed it is in host mode hprt0 = 00001101
[ 1.114192] EXT4-fs (mmcblk0p2): orphan cleanup on readonly fs
[ 1.114327] EXT4-fs (mmcblk0p2): 1 orphan inode deleted
[ 1.114333] EXT4-fs (mmcblk0p2): recovery complete
[ 1.123189] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.123245] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 1.131017] devtmpfs: mounted
[ 1.134031] Freeing unused kernel memory: 1024K
[ 1.311803] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[ 1.311818] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 1.312429] hub 1-1:1.0: USB hub found
[ 1.312513] hub 1-1:1.0: 4 ports detected
[ 1.507712] systemd[1]: System time before build time, advancing clock.
[ 1.631593] usb 1-1.1: new high-speed USB device number 3 using dwc_otg
[ 1.638858] NET: Registered protocol family 10
[ 1.640026] Segment Routing with IPv6
[ 1.649127] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.666272] random: systemd: uninitialized urandom read (16 bytes read)
[ 1.678070] systemd[1]: systemd 232 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN)
[ 1.678604] systemd[1]: Detected architecture arm.
[ 1.679447] systemd[1]: Set hostname to .
[ 1.711361] random: systemd: uninitialized urandom read (16 bytes read)
[ 1.732156] random: systemd-cryptse: uninitialized urandom read (16 bytes read)
[ 1.761871] usb 1-1.1: New USB device found, idVendor=0424, idProduct=2514
[ 1.761886] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 1.762510] hub 1-1.1:1.0: USB hub found
[ 1.762613] hub 1-1.1:1.0: 3 ports detected
[ 2.115544] dwc_otg_handle_wakeup_detected_intr lxstate = 2
[ 2.124665] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 2.125049] systemd[1]: Listening on fsck to fsckd communication Socket.
[ 2.125307] systemd[1]: Listening on Syslog Socket.
[ 2.125550] systemd[1]: Listening on udev Kernel Socket.
[ 2.126283] systemd[1]: Created slice System Slice.
[ 2.128864] systemd[1]: Mounting RPC Pipe File System…
[ 2.132874] systemd[1]: Mounting POSIX Message Queue File System…
[ 2.266917] i2c /dev entries driver
[ 2.274516] dwm: no symbol version for module_layout
[ 2.274544] dwm: loading out-of-tree module taints kernel.
[ 2.582854] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 2.591596] usb 1-1.1.1: new high-speed USB device number 4 using dwc_otg
[ 2.677830] systemd-journald[88]: Received request to flush runtime journal from PID 1
[ 2.722190] usb 1-1.1.1: New USB device found, idVendor=0424, idProduct=7800
[ 2.722207] usb 1-1.1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.996613] libphy: lan78xx-mdiobus: probed
[ 3.212595] dwm spi0.0: loading
[ 3.212833] dwm spi0.0: DWM1001 TWR Real Time Location System
[ 3.212844] dwm spi0.0:
[ 3.212853] dwm spi0.0: Copyright : 2016-2019 LEAPS and Decawave
[ 3.212861] dwm spi0.0: License : Please visit DWM1001, DW10001-DEV and MDEK1001 Documents, Source Code, Android Application & R2.0 Firmware Image - Decawave
[ 3.212869] dwm spi0.0: Compiled : Feb 4 2019 12:36:58
[ 3.313201] snd_bcm2835: module is from the staging directory, the quality is unknown, you have been warned.
[ 3.318332] bcm2835_alsa bcm2835_alsa: card created with 8 channels
[ 3.501873] brcmfmac: F1 signature read @0x18000000=0x15264345
[ 3.511774] brcmfmac: brcmf_fw_map_chip_to_name: using brcm/brcmfmac43455-sdio.bin for chip 0x004345(17221) rev 0x000006
[ 3.512282] usbcore: registered new interface driver brcmfmac
[ 3.973655] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 3.973683] dwm spi0.0: dwm_node_id_get failed, error -12
[ 3.973695] dwm spi0.0: reseting bridge
[ 4.171709] random: crng init done
[ 4.171721] random: 7 urandom warning(s) missed due to ratelimiting
[ 4.225005] brcmfmac: brcmf_c_preinit_dcmds: Firmware version = wl0: Feb 27 2018 03:15:32 version 7.45.154 (r684107 CY) FWID 01-4fbe0b04
[ 4.225586] brcmfmac: brcmf_c_preinit_dcmds: CLM version = API: 12.2 Data: 9.10.105 Compiler: 1.29.4 ClmImport: 1.36.3 Creation: 2018-03-09 18:56:28
[ 4.527627] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 4.527652] dwm spi0.0: dwm_reset failed, error -14
[ 4.527660] dwm spi0.0: bridge can’t be initialized, error -14
[ 5.364277] uart-pl011 3f201000.serial: no DMA platform data
[ 5.995776] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 5.995794] brcmfmac: power management disabled
[ 6.057318] Adding 102396k swap on /var/swap. Priority:-2 extents:1 across:102396k SSFS
[ 6.231633] Under-voltage detected! (0x00050005)
[ 6.415297] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 6.607595] dwm spi0.0: PAN ID changed by user to x783A
[ 6.607611] dwm spi0.0: encryption key changed by user
[ 6.607619] dwm spi0.0: encryption configuration changed by user
[ 6.607627] dwm spi0.0: firmware update configuration changed by user
[ 6.607634] dwm spi0.0: UWB mode configuration changed by user
[ 6.607642] dwm spi0.0: reinitialize …
[ 6.607651] dwm spi0.0: can’t schedule work: BH start reinit
[ 7.967524] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[ 8.314660] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 8.314681] dwm spi0.0: dwm_node_id_get failed, error -12
[ 8.314691] dwm spi0.0: reseting bridge
[ 8.854632] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 8.854652] dwm spi0.0: dwm_reset failed, error -14
[ 8.854660] dwm spi0.0: bridge can’t be initialized, error -14
[ 11.338560] fuse init (API version 7.26)
[ 12.025730] Bluetooth: Core ver 2.22
[ 12.025812] NET: Registered protocol family 31
[ 12.025818] Bluetooth: HCI device and connection manager initialized
[ 12.025840] Bluetooth: HCI socket layer initialized
[ 12.025854] Bluetooth: L2CAP socket layer initialized
[ 12.025888] Bluetooth: SCO socket layer initialized
[ 12.041461] Bluetooth: HCI UART driver ver 2.3
[ 12.041571] Bluetooth: HCI UART protocol H4 registered
[ 12.041577] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 12.041808] Bluetooth: HCI UART protocol Broadcom registered
[ 12.645175] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 12.645198] dwm spi0.0: dwm_node_id_get failed, error -12
[ 12.645207] dwm spi0.0: reseting bridge
[ 12.781558] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 12.781571] Bluetooth: BNEP filters: protocol multicast
[ 12.781590] Bluetooth: BNEP socket layer initialized
[ 12.897090] Bluetooth: RFCOMM TTY layer initialized
[ 12.897122] Bluetooth: RFCOMM socket layer initialized
[ 12.897146] Bluetooth: RFCOMM ver 1.11
[ 13.233274] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 13.233288] dwm spi0.0: reseting bridge manually
[ 13.233406] dwm spi0.0: dwm_reset failed, error -14
[ 13.233415] dwm spi0.0: bridge can’t be initialized, error -14
[ 17.054264] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 17.054278] dwm spi0.0: reseting bridge manually
[ 17.054394] dwm spi0.0: dwm_node_id_get failed, error -12
[ 17.054403] dwm spi0.0: reseting bridge
[ 17.590941] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 17.590948] dwm spi0.0: reseting bridge manually
[ 17.591056] dwm spi0.0: dwm_reset failed, error -14
[ 17.591060] dwm spi0.0: bridge can’t be initialized, error -14
[ 21.354094] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 21.354108] dwm spi0.0: reseting bridge manually
[ 21.354224] dwm spi0.0: dwm_node_id_get failed, error -12
[ 21.354234] dwm spi0.0: reseting bridge
[ 21.894122] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 21.894134] dwm spi0.0: reseting bridge manually
[ 21.894249] dwm spi0.0: dwm_reset failed, error -14
[ 21.894257] dwm spi0.0: bridge can’t be initialized, error -14
[ 24.951568] Voltage normalised (0x00000000)
[ 25.668931] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 25.668940] dwm spi0.0: reseting bridge manually
[ 25.669049] dwm spi0.0: dwm_node_id_get failed, error -12
[ 25.669054] dwm spi0.0: reseting bridge
[ 26.198042] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 26.198050] dwm spi0.0: reseting bridge manually
[ 26.198159] dwm spi0.0: dwm_reset failed, error -14
[ 26.198162] dwm spi0.0: bridge can’t be initialized, error -14
[ 29.988749] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 29.988757] dwm spi0.0: reseting bridge manually
[ 29.988866] dwm spi0.0: dwm_node_id_get failed, error -12
[ 29.988870] dwm spi0.0: reseting bridge
[ 30.518055] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 30.518062] dwm spi0.0: reseting bridge manually
[ 30.518170] dwm spi0.0: dwm_reset failed, error -14
[ 30.518173] dwm spi0.0: bridge can’t be initialized, error -14
[ 34.310479] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 34.310487] dwm spi0.0: reseting bridge manually
[ 34.310597] dwm spi0.0: dwm_node_id_get failed, error -12
[ 34.310602] dwm spi0.0: reseting bridge
[ 34.838052] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 34.838060] dwm spi0.0: reseting bridge manually
[ 34.838168] dwm spi0.0: dwm_reset failed, error -14
[ 34.838172] dwm spi0.0: bridge can’t be initialized, error -14
[ 35.351787] Under-voltage detected! (0x00050005)
[ 38.630062] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 38.630071] dwm spi0.0: reseting bridge manually
[ 38.630182] dwm spi0.0: dwm_node_id_get failed, error -12
[ 38.630188] dwm spi0.0: reseting bridge
[ 39.163139] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 39.163151] dwm spi0.0: reseting bridge manually
[ 39.163266] dwm spi0.0: dwm_reset failed, error -14
[ 39.163274] dwm spi0.0: bridge can’t be initialized, error -14
[ 42.949541] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 42.949548] dwm spi0.0: reseting bridge manually
[ 42.949656] dwm spi0.0: dwm_node_id_get failed, error -12
[ 42.949660] dwm spi0.0: reseting bridge
[ 43.478056] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 43.478064] dwm spi0.0: reseting bridge manually
[ 43.478175] dwm spi0.0: dwm_reset failed, error -14
[ 43.478179] dwm spi0.0: bridge can’t be initialized, error -14
[ 45.751567] Voltage normalised (0x00000000)
[ 47.269541] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 47.269549] dwm spi0.0: reseting bridge manually
[ 47.269656] dwm spi0.0: dwm_node_id_get failed, error -12
[ 47.269661] dwm spi0.0: reseting bridge
[ 47.798043] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 47.798049] dwm spi0.0: reseting bridge manually
[ 47.798157] dwm spi0.0: dwm_reset failed, error -14
[ 47.798160] dwm spi0.0: bridge can’t be initialized, error -14
[ 51.589378] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 51.589388] dwm spi0.0: reseting bridge manually
[ 51.589495] dwm spi0.0: dwm_node_id_get failed, error -12
[ 51.589499] dwm spi0.0: reseting bridge
[ 52.118031] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 52.118039] dwm spi0.0: reseting bridge manually
[ 52.118147] dwm spi0.0: dwm_reset failed, error -14
[ 52.118150] dwm spi0.0: bridge can’t be initialized, error -14
[ 55.909344] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 55.909352] dwm spi0.0: reseting bridge manually
[ 55.909461] dwm spi0.0: dwm_node_id_get failed, error -12
[ 55.909465] dwm spi0.0: reseting bridge
[ 56.438019] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 56.438026] dwm spi0.0: reseting bridge manually
[ 56.438134] dwm spi0.0: dwm_reset failed, error -14
[ 56.438137] dwm spi0.0: bridge can’t be initialized, error -14
[ 60.229169] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 60.229176] dwm spi0.0: reseting bridge manually
[ 60.229285] dwm spi0.0: dwm_node_id_get failed, error -12
[ 60.229289] dwm spi0.0: reseting bridge
[ 60.758049] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 60.758056] dwm spi0.0: reseting bridge manually
[ 60.758164] dwm spi0.0: dwm_reset failed, error -14
[ 60.758168] dwm spi0.0: bridge can’t be initialized, error -14
[ 64.549130] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 64.549139] dwm spi0.0: reseting bridge manually
[ 64.549248] dwm spi0.0: dwm_node_id_get failed, error -12
[ 64.549253] dwm spi0.0: reseting bridge
[ 65.078019] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 65.078025] dwm spi0.0: reseting bridge manually
[ 65.078133] dwm spi0.0: dwm_reset failed, error -14
[ 65.078137] dwm spi0.0: bridge can’t be initialized, error -14
[ 68.873123] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 68.873133] dwm spi0.0: reseting bridge manually
[ 68.873241] dwm spi0.0: dwm_node_id_get failed, error -12
[ 68.873245] dwm spi0.0: reseting bridge
[ 69.418224] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 69.418231] dwm spi0.0: reseting bridge manually
[ 69.418338] dwm spi0.0: dwm_reset failed, error -14
[ 69.418342] dwm spi0.0: bridge can’t be initialized, error -14
[ 73.189613] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 73.189621] dwm spi0.0: reseting bridge manually
[ 73.189729] dwm spi0.0: dwm_node_id_get failed, error -12
[ 73.189733] dwm spi0.0: reseting bridge
[ 73.718964] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 73.718972] dwm spi0.0: reseting bridge manually
[ 73.719080] dwm spi0.0: dwm_reset failed, error -14
[ 73.719084] dwm spi0.0: bridge can’t be initialized, error -14
[ 77.515475] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 77.515487] dwm spi0.0: reseting bridge manually
[ 77.515603] dwm spi0.0: dwm_node_id_get failed, error -12
[ 77.515612] dwm spi0.0: reseting bridge
[ 78.049844] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 78.049858] dwm spi0.0: reseting bridge manually
[ 78.049974] dwm spi0.0: dwm_reset failed, error -14
[ 78.049982] dwm spi0.0: bridge can’t be initialized, error -14
[ 79.033212] Under-voltage detected! (0x00050005)
[ 81.831150] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 81.831158] dwm spi0.0: reseting bridge manually
[ 81.831265] dwm spi0.0: dwm_node_id_get failed, error -12
[ 81.831269] dwm spi0.0: reseting bridge
[ 82.359945] dwm spi0.0: decode TLV failed, error 2 t:0 l:0
[ 82.359952] dwm spi0.0: reseting bridge manually
[ 82.360060] dwm spi0.0: dwm_reset failed, error -14