Hi Brock,
For some reason the compiler is not understanding the the * as a wildcard.
As a workaround we did the following, and it worked for us:
In the ‘Project Explorer’ pane of SES, right click on the Solution and select ‘Options…’
In the Code/External Build section is the Link Command. You will need to edit a part in the middle of this.
Find the snippet that says:
“$(SolutionDir)/output/compiler/*.o”
and edit it to say:
“$(SolutionDir)/output/compiler/$(SolutionName).o”
Leaving all the rest of the command as it is.
Hope it helps,
Ryan