Hello!
I have a question regarding the passive/listener mode. I have a MDEK1001 kit on order, so I am preparing an application for a host (single board) computer.
In my setup I will use the DWM1001-DEV boards as 4 anchors, 2-6 tags and 1 “listener”. I want to get all tags positions via the listener node, using the generic UART API.
In the documentation (MDEk1001 User Manual) I can only find an example of using the shell mode for a passive/listener node. I.e. sending the “les” or “lec” command to the listener over UART, it will respond with the address and position of all tags it can hear (right?).
In generic mode, will the dwm_loc_get (API Guide 4.3.9.3) do the same thing? I.e. If I send this TLV request to the listener the response will be addresses and positions of several tags? In the API guide it seems like the corresponding response only includes distances and positions of several anchors, not tags. Am I missing anything?
The answer to my question might be obvious when my HW is delivered and up and running, but I am eager to start implementing as much as possible in beforehand. I will write the host side application in python.
Br,
Rark