I have three modules ( 1tag and 2 anchor) I would like to have the positon X of the tag but I have some difficulties. First I flash the 3 modules with J-Flash Link,I use the application to configure the modules, after I use Segger Studio to build and run dwm-simple after I connect the tag to the raspberry pi 3 B+, I connect with serial connection in to raspberry , its works but when I enter les or lec is not work not information about the position or distance. Can you help me please ?
Thanks Yves for you reply,
At the moment I have just 3 modules, I do use which file ? Hex PANNS ??
The serial connection function with raspberry but when I use the command lec I don’t have data. There are no connection between tag and anchor.
which Raspberry Image have you used? If you use the image from PANS, then that image is intended to be used as a Gateway. It will automatically configure the connected DWM1001-DEV to Bridge mode.
You can disable the Gateway function as follow:
$ sudo /etc/init.d/dwm1001-proxy stop
$ sudo /etc/init.d/dwm1001 stop
$ sudo rmmod dwm
By doing that you will take control over the connected module.
If your Raspberry image is not from PANS, then follow Yves’s instructions. Providing the output of ‘si’ and ‘la’ commands on the Tag should help.