I am in need of the DWM1001-DEV segger code so that I can build the project on a modified NFR52832 board
I am trying the same thing. There are SES examples in the source code download under the DMM1001-DEV product page; but, as far as I can tell they are for RTLS and assume a configuration of anchors that are setup using TWR. I also tried using using the Nordic nRF5 SDK examples directly and was not able to get them to work with the DMM1001-DEV.