I have brought MDEK1001 module, out of which I was using 4 modules as anchors, 1 as tag and 1 I was trying to make bridge node using the raspberry image. All of the module was getting detected and was configurable over BLE in android app. Suddenly, one of them is not getting detected in android app, but I am able to change its mode over uart. I made the not working one as tag. Now to understand is there settings issue , I see the details of working tag module and not working bridge module which is now made tag module as well, using si command.
I attaching the two screen shots. Only difference I could see is stat_det=1 (sens=1) part , what does this mean, has my module gone bad ?
Any inputs would be helpful. Thank you.
Screen Shots(Merged)