Is´t possible to activate “LEP ON” with PANS2 whitout any other Arduino or Raspberry Pi units connected to my DWM1001-DEV card?
Hi @MacTommy
no that’s not possible.
Cheers
JK
Thanks for that. It was a shame that I don’t have that option for the “tracker”, when the anchor works fine without activating anything more than activating the Tracker-function in CLI. If I have done all the settings etc. and then just need to activate “lep on” and I will need a “whole” Arduino just for that.
It sounds like I should skip the DWM1001-DEV and just run the DWM1001C and a Seeeduino XIAO sense. Should be able to be a smaller unit even if you add a module for charging the battery.
How do you update PANS on a DWM1001C? Because that’s what “J-Link On-Board” does for me? Maybee I start a new question for that.
Hi @MacTommy
in most cases you need programmer or DRTLS app. If it is already flashed with PANS 2.0 and you wan to distribute an updated app with your own library on then you just need enable the FW update on all nodes. And then only program the initiator with new FW and it will be automatically distrubuted across the network.
Cheers
JK