Hello,
I’ve successfully installed the firmware on my DWM1001 modules, but I’m encountering an issue where the Anchor and Tag modules are not connecting properly. Below are the details of the setup and the troubleshooting steps I’ve followed:
Setup:
• 3 Anchor modules and 1 Tag module .
• I have configured all modules with the same Network ID (0x1234) using the dwm> nis 0x1234 command.
• Each module has been set to the correct mode:
• Anchors: dwm> nma
• Tag: dwm> nmt
Issue:
• When I check the list of Anchors using la, I see no Anchors listed (only cnt=0).
• The les command on the Tag module gives no response.