#if CONFIG_SOC_NRF52833 || CONFIG_SOC_NRF52840
// JC #if CONFIG_SHIELD_QORVO_DWS3000
#if CONFIG_DW3000
/* Due to the wiring of the Nordic Development Boards and the DWS3000
* Arduino shield it is not possible to use more than 16MHz */
spi_cfgs[1].frequency = 16000000;
#else
spi_cfgs[1].frequency = 32000000;
#endif
In dw_30000_spi.c is the wrong config value of CONFIG_SHIELD_QORVO_DWS3000 used ?
I’m trying to see a range using initiator and responder, but at the moment I get nothing.