Hi Qorvo team,
I used DWT_PHRMODE_EXT to transmit longer frames but DW3000 sent the wrong frames for lengths over 256 bytes.
Here is the configuration of DW3000.
static dwt_config_t config = {
5, /* Channel number. */
DWT_PLEN_1024, /* Preamble length. Used in TX only. */
DWT_PAC32, /* Preamble acquisition chunk size. Used in RX only. */
9, /* TX preamble code. Used in TX only. */
9, /* RX preamble code. Used in RX only. */
0, /* 0 to use standard 8 symbol SFD, 1 to use non-standard 8 symbol, 2 for non-standard 16 symbol SFD and 3 for 4z 8 symbol SDF type */
DWT_BR_850K, /* Data rate. */
//DWT_PHRMODE_STD, /* PHY header mode. */
DWT_PHRMODE_EXT,
DWT_PHRRATE_STD, /* PHY header rate. */
(1024 + 1 + 8 - 32),/* SFD timeout (preamble length + 1 + SFD length - PAC size). Used in RX only. */
DWT_STS_MODE_OFF, /* No STS mode enabled (STS Mode 0). */
DWT_STS_LEN_64, /* STS length, see allowed values in Enum dwt_sts_lengths_e */
DWT_PDOA_M0 /* PDOA mode off */
};
This is what I trying to transmit, it is a total of 294bytes without FCS_LEN.
static uint8_t tx_msg[] = {
0xC5, 0, 'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A', 'W', 'A', 'V', 'E',
'D', 'E', 'C', 'A'
};
However, DW3000 received the wrong frame, as shown in the picture below.

I tried using DW1000 to transmit the same frame, and DW3000 received the correct frame, indicating a tx bug.
Is there any way to fix this problem?