I’m selecting a chip for a project that requires support for direction finding. We’re currently looking at the DW3110 and DW3120.
I’m a bit confused about the requirements for this. The DW3120 states that it supports PDoA and TDoA since it has two antenna ports, which makes sense. However, the DW3110 also states that it supports PDoA and TDoA; how is this possible when it only supports a single antenna? Aren’t two antennas needed for that?
I’m also curious if any of the products support 3-dimensional Angle of Arrival (elevation and azimuth). Are there any configurations that would support this (e.g. a DW3120 with one antenna on one port, and a switch between two other antennas on the second port), and if so, are there any firmware examples?