DW3 QM33 SDK v1.1.1 build (uci, Murata Type2AB) on mac, uint8_t and int16_t undefined

DW3_QM33_SDK_1.1.1/SDK/Firmware/DW3_QM33_SDK_1.1.1/Src/Helpers/Inc/uwb_convert.h:18:30: error: unknown type name ‘uint8_t’
18 | float convert_rssi_q7_to_dbm(uint8_t rssi_q7);

DW3_QM33_SDK_1.1.1/SDK/Firmware/DW3_QM33_SDK_1.1.1/Src/Helpers/uwb_convert.c:15:34: error: unknown type name ‘int16_t’
15 | float convert_aoa_2pi_q16_to_deg(int16_t aoa_2pi_q16)

had to add

#include <stdint.h> 

to the uwb_convert.h