I have a network set up with 4 anchors and 2 tags, along with one listener tag.
As the current C API doesn’t seem to provide interfaces for the listener mode, I currently utilise the shell mode les command. However, I am having trouble understanding the output.
Questions:
Are the [x,y,z,quality] reported by the tags in the same units as the TLV position variable? i.e in millimetres?
The optional distance reported is to the listener tag?
On the first line :
[list]
[*][size=medium][font=Arial]1897.830 time stamp in s[/font][/size]
[/list]
On the second line:
[list]
[]CD1A --> Tag name
[]1.23 --> X coordinate in m
[]1.31 --> Y coordinate in m
[]1.32 --> Z coordinate in m
[]0 --> Quality factor in percent (from 0 to 100)
[]xCC -> sample counter
[/list]
What are you referring to with the “optional distance” ?
Thanks for the explanation. The optional distance was from misinterpreting the line “Show distances to ranging anchors and the position if location engine is enabled.” from the API-guide. But you have cleared that up in the other thread, thanks!
About the tag names field - they don’t seem to correspond to the names set in the Android app?
It would seem that the name is the panidthat the tag is assigned in the network. Unfortunately, I don’t see how to determine which a tags’s panid other than via the UART shell with the System info si command.