When I initialized the chip dw1000, the initialization failed.
Is there a good way of checking .
THANKS
When I initialized the chip dw1000, the initialization failed.
Is there a good way of checking .
THANKS
please provide more details:
HW ?
SW ?
steps to make issue happen…
I use the STM32C8T6 to controled the DW1000 via SPI interface。and use the “inittestapplication(uint8 s1switch)” to init the dw1000.but i don’t success.
[code]uint32 inittestapplication(uint8 s1switch)
{
uint32 devID ;
instanceConfig_t instConfig;
int result;
SPI_ConfigFastRate(SPI_BaudRatePrescaler_32); //max SPI before PLLs configured is ~4M
//this is called here to wake up the device (i.e. if it was in sleep mode before the restart)
devID = instancereaddeviceid() ;
if(DWT_DEVICE_ID != devID) //if the read of device ID fails, the DW1000 could be asleep
{
port_SPIx_clear_chip_select(); //CS low
Sleep(1); //200 us to wake up then waits 5ms for DW1000 XTAL to stabilise
port_SPIx_set_chip_select(); //CS high
Sleep(7);
devID = instancereaddeviceid() ;
// SPI not working or Unsupported Device ID
if(DWT_DEVICE_ID != devID)
return(-1) ;
//clear the sleep bit - so that after the hard reset below the DW does not go into sleep
dwt_softreset();
}
//reset the DW1000 by driving the RSTn line low
reset_DW1000();
result = instance_init() ;
if (0 > result) return(-1) ; // Some failure has occurred
SPI_ConfigFastRate(SPI_BaudRatePrescaler_4); //increase SPI to max
devID = instancereaddeviceid() ;
if (DWT_DEVICE_ID != devID) // Means it is NOT DW1000 device
{
// SPI not working or Unsupported Device ID
return(-1) ;
}
if((s1switch & SWS1_ANC_MODE) == 0)
{
instance_mode = TAG;
}
else
{
instance_mode = ANCHOR;
}
addressconfigure(s1switch, instance_mode) ; // set up initial payload configuration
if((instance_mode == ANCHOR) && (instance_anchaddr > 0x3))
{
instance_mode = LISTENER;
}
instancesetrole(instance_mode) ; // Set this instance role
// get mode selection (index) this has 4 values see chConfig struct initialiser for details.
dr_mode = decarangingmode(s1switch);
chan = instConfig.channelNumber = chConfig[dr_mode].channel ;
instConfig.preambleCode = chConfig[dr_mode].preambleCode ;
instConfig.pulseRepFreq = chConfig[dr_mode].prf ;
instConfig.pacSize = chConfig[dr_mode].pacSize ;
instConfig.nsSFD = chConfig[dr_mode].nsSFD ;
instConfig.sfdTO = chConfig[dr_mode].sfdTO ;
instConfig.dataRate = chConfig[dr_mode].datarate ;
instConfig.preambleLen = chConfig[dr_mode].preambleLength ;
instance_config(&instConfig, &sfConfig[dr_mode]) ; // Set operating channel etc
return devID;
}[/code]
So you are using EVB1000 (EVK) code on your own HW?
Please have a look as APS022 Application Note (Debugging)
As a first step, you should power on the IC/micro, then configure/initialise micro’s SPI and then check SPI is working correctly, just by reading from register 0 - to check if you get 0xdeca0130.
If the SPI is working correctly, then move onto application…
Please also search the forum, there are a lot of other threads which discuss SPI configurations and issues, and how to resolve them.
Thank you very much
![]()