Hi,
I had the chance to check the waveform of a DWM1000 module.
In upfront, I did following checks:
- Reset DWM100
- Setup registers as per DW1000 users manual 2.10 chapter 8.1.1 (page 189), the only difference is that I used values for CH3 instead of CH5
Here’s my plot of DWM1000 which I expect to be factory calibrated (isn’t it?)
So, the same dip in the middle of band and slightly different center freq compared to my previous post with DW1000 and custom PCB. I put marker to the nominal center which is 4492.8MHz but I can consider this deviation as missing calibration of my spectrum.
I also took a screenshot with more span, in this one it is 200MHz:
This is still the DWM1000 and I also see the harmonics in ± 38.4MHz which makes me suspicious of intermodulation with clock signal.
I’m unsure if this is what I should see but I can confirm that this DWM1000 tag works perfectly in non-test conditions.
I’m a bit lost…
Do I have measurement errors? Or should anything else configured for test mode than description mentioned in users manual above?
Anyone from DW, do you have guys some reference plots I could compare my one?
Any thoughts or hints are much appreciated.
Thanks,
d