Hi all,
I’ve been trying to use SS TWR example with an SAM4S chip and noticed that whenever I try reading any registers with an offset using the DW1000 API, I consistently get 0xDEDE or 0xDE. I’ve read in the User Manual that any unused or reserved registers return 0xDEAD. However this shouldn’t be the case as the only times I am reading registers at an offset are in the supplied API such as dwt_starttx and dwt_readcarrierintegrator.
I doubt this is an SPI issue as every other register read works perfectly fine. The only change I made to dwt_starttx was to only check for HPDWARN, as even if TXPUTE was flagged, frame transmission will still continue. The definitions for 2 API functions I have issues with are posted below.


int dwt_starttx(uint8 mode)
{
int retval = DWT_SUCCESS ;
uint8 temp = 0x00;
uint16 checkTxOK = 0 ;
if (mode & DWT_RESPONSE_EXPECTED)
{
temp = (uint8)SYS_CTRL_WAIT4RESP ; // Set wait4response bit
pdw1000local->wait4resp = 1;
}
if (mode & DWT_START_TX_DELAYED)
{
// Both SYS_CTRL_TXSTRT and SYS_CTRL_TXDLYS to correctly enable TX
temp |= (uint8)(SYS_CTRL_TXDLYS | SYS_CTRL_TXSTRT);
dwt_write8bitoffsetreg(SYS_CTRL_ID, SYS_CTRL_OFFSET, temp);
uint16 txpute = dwt_read8bitoffsetreg(DIG_DIAG_ID, EVC_TPW_OFFSET); // offset 0x1A
uint16 hpdwarn = dwt_read8bitoffsetreg(DIG_DIAG_ID, EVC_HPW_OFFSET); //offset 0x18
checkTxOK = dwt_read16bitoffsetreg(SYS_STATUS_ID, 3); // offset 3 to get the upper 2 bytes
uint32 check = dwt_read32bitoffsetreg(SYS_STATUS_ID, 0);
if ((check & SYS_STATUS_HPDWARN) == 1) // Transmit Delayed Send set over Half a Period away or Power Up error (there is enough time to send but not to power up individual blocks).
{
// If HPDWARN or TXPUTE are set this indicates that the TXDLYS was set too late for the specified DX_TIME.
// remedial action is to cancel delayed send and report error
dwt_write8bitoffsetreg(SYS_CTRL_ID, SYS_CTRL_OFFSET, (uint8)SYS_CTRL_TRXOFF);
printf("FAILED HPDWARN TRIGGERED\r\n");
retval = DWT_ERROR ; //Failed!
}
else //we bypass the err bc HPDWARN not triggered and TXPUTE cant read atm
//TXPUTE is not enough to completely stop the transmission in but HPDWARN is
{
retval = DWT_SUCCESS ; // may still have TXPUTE
}
}
else
{
temp |= (uint8)SYS_CTRL_TXSTRT ;
dwt_write8bitoffsetreg(SYS_CTRL_ID, SYS_CTRL_OFFSET, temp);
dwt_read32bitreg(SYS_CTRL_ID);
dwt_read32bitreg(SYS_STATE_ID);
}
return retval;
} // end dwt_starttx()
int32 dwt_readcarrierintegrator(void)
{
uint32 regval = 0 ;
int j ;
uint8 buffer[DRX_CARRIER_INT_LEN] ;
/* Read 3 bytes into buffer (21-bit quantity) */
dwt_readfromdevice(DRX_CONF_ID, DRX_CARRIER_INT_OFFSET, DRX_CARRIER_INT_LEN, buffer) ; //offset 0x28
for (j = 2 ; j >= 0 ; j --) // arrange the three bytes into an unsigned integer value
{
regval = (regval << 8) + buffer[j] ;
}
if (regval & B20_SIGN_EXTEND_TEST) {
regval |= B20_SIGN_EXTEND_MASK ; // sign extend bit #20 to whole word
}
else {
regval &= DRX_CARRIER_INT_MASK ; // make sure upper bits are clear if not sign extending
}
return (int32) regval ; // cast unsigned value to signed quantity.
}