Hello, I used DW1000 to conduct 4 base stations and 1 tag for positioning. But the frequency of measurement data I get is very low, and it takes about 90ms for the tag to get the distance to four base stations. The update frequency of distance data measured by the label is about 12HZ. May I ask whether this is a normal situation? How many HZ can the maximum position update frequency of DW1000 be?
Hi @lange.you
Im not sure to what SW you are referring to.
The update rate and other staff purely depends on on used firmware. For example for the PANS firmware the maximum update rate is 10Hz. Some other firmware can do much higher update rates.
Cheers
JK