Could I ask what you have tried yourself eg by using example code 3a and what results have you seen?
Would you have tried this by setting msgp5 and msgp6 into mode 1 to see the EXTTXE and EXTRXE signals onto a scope ?
thanks for your reply.
we have tested GPIO4&5&6 on the scope by setting MSGP4&5&6 to mode 1.
and the result is as below.
test condition:
Hardware: TTK1000 anchor board.
Source code :TTK1000_Release_1.1
test time: capturing tx burst start。(150ms CCP)
GPIO4 will be high earllier 8ns than GOIP5。
if we use GPIO4 to control the power on/off of a extPA, 8ns is enough or not?
we have choosed GALI-39+ of Mini-Circuits for supporting channel 2&5 at the same time.
HMC326 has a enable pin, but his frequency is only at 3.0-4.5GHZ.