Q_Nerk
March 17, 2022, 8:43pm
1
Hello,
I started work with DW1000.
I connected it to ESP32 (Healtec with Lora).
I’ve uploaded to ESP32 for tag:
#include <SPI.h>
#include "DW1000Ranging.h"
#define SPI_SCK 18
#define SPI_MISO 19
#define SPI_MOSI 23
#define DW_CS 4
// connection pins
const uint8_t PIN_RST = 27; // reset pin
const uint8_t PIN_IRQ = 34; // irq pin
const uint8_t PIN_SS = 5; // spi select pin
void setup()
{
Serial.begin(115200);
delay(1000);
//init the configuration
SPI.begin(SPI_SCK, SPI_MISO, SPI_MOSI);
DW1000Ranging.initCommunication(PIN_RST, PIN_SS, PIN_IRQ); //Reset, CS, IRQ pin
//define the sketch as anchor. It will be great to dynamically change the type of module
DW1000Ranging.attachNewRange(newRange);
DW1000Ranging.attachNewDevice(newDevice);
DW1000Ranging.attachInactiveDevice(inactiveDevice);
//Enable the filter to smooth the distance
//DW1000Ranging.useRangeFilter(true);
//we start the module as a tag
DW1000Ranging.startAsTag("7D:00:22:EA:82:60:3B:9C", DW1000.MODE_LONGDATA_RANGE_LOWPOWER);
}
void loop()
{
DW1000Ranging.loop();
}
void newRange()
{
Serial.print("from: ");
Serial.print(DW1000Ranging.getDistantDevice()->getShortAddress(), HEX);
Serial.print("\t Range: ");
Serial.print(DW1000Ranging.getDistantDevice()->getRange());
Serial.print(" m");
Serial.print("\t RX power: ");
Serial.print(DW1000Ranging.getDistantDevice()->getRXPower());
Serial.println(" dBm");
}
void newDevice(DW1000Device *device)
{
Serial.print("ranging init; 1 device added ! -> ");
Serial.print(" short:");
Serial.println(device->getShortAddress(), HEX);
}
void inactiveDevice(DW1000Device *device)
{
Serial.print("delete inactive device: ");
Serial.println(device->getShortAddress(), HEX);
}
and second unit for anchor:
#include <SPI.h>
#include "DW1000Ranging.h"
#define ANCHOR_ADD "83:17:5B:D5:A9:9A:E2:9C"
#define SPI_SCK 18
#define SPI_MISO 19
#define SPI_MOSI 23
#define DW_CS 4
// connection pins
const uint8_t PIN_RST = 27; // reset pin
const uint8_t PIN_IRQ = 34; // irq pin
const uint8_t PIN_SS = 4; // spi select pin
void setup() {
Serial.begin(115200);
delay(1000);
//init the configuration
DW1000Ranging.initCommunication(PIN_RST, PIN_SS, PIN_IRQ); //Reset, CS, IRQ pin
//define the sketch as anchor. It will be great to dynamically change the type of module
DW1000Ranging.attachNewRange(newRange);
DW1000Ranging.attachBlinkDevice(newBlink);
DW1000Ranging.attachInactiveDevice(inactiveDevice);
//Enable the filter to smooth the distance
//DW1000Ranging.useRangeFilter(true);
//we start the module as an anchor
DW1000Ranging.startAsAnchor("82:17:5B:D5:A9:9A:E2:9C", DW1000.MODE_LONGDATA_RANGE_ACCURACY);
}
void loop() {
DW1000Ranging.loop();
}
void newRange() {
Serial.print("from: "); Serial.print(DW1000Ranging.getDistantDevice()->getShortAddress(), HEX);
Serial.print("\t Range: "); Serial.print(DW1000Ranging.getDistantDevice()->getRange()); Serial.print(" m");
Serial.print("\t RX power: "); Serial.print(DW1000Ranging.getDistantDevice()->getRXPower()); Serial.println(" dBm");
}
void newBlink(DW1000Device* device) {
Serial.print("blink; 1 device added ! -> ");
Serial.print(" short:");
Serial.println(device->getShortAddress(), HEX);
}
void inactiveDevice(DW1000Device* device) {
Serial.print("delete inactive device: ");
Serial.println(device->getShortAddress(), HEX);
}
And in serial monitor I see only ID + named TAG or Anchor. How to reach distance between tag and anchor? Connections are direct between DW1000 and ESP32
hello, do you solve the problem?
I have the same problem, I do not have any message in serial.
Hello. Are you sure connected all the pins ? If you connect all of them, the problem will be solved.
Q_Nerk:
#define DW_CS 4
In addition #define DW_CS 4 is not correct. You should change it as 5.
Were you able to solve it? I have the same issue, the only message I get the ID and wether it’s a tag or an anchor
Yes, I’ve fixed it:
#include <SPI.h>
#include <DW1000.h>
#define SPI_SCK 18
#define SPI_MISO 19
#define SPI_MOSI 23
#define DW_CS 4
// connection pins
const uint8_t PIN_RST = 27; // reset pin
const uint8_t PIN_IRQ = 34; // irq pin
const uint8_t PIN_SS = 4; // spi select pin
// messages used in the ranging protocol
// TODO replace by enum
#define POLL 0
#define POLL_ACK 1
#define RANGE 2
#define RANGE_REPORT 3
#define RANGE_FAILED 255
// message flow state
volatile byte expectedMsgId = POLL_ACK;
// message sent/received state
volatile boolean sentAck = false;
volatile boolean receivedAck = false;
// timestamps to remember
DW1000Time timePollSent;
DW1000Time timePollAckReceived;
DW1000Time timeRangeSent;
// data buffer
#define LEN_DATA 16
byte data[LEN_DATA];
// watchdog and reset period
uint32_t lastActivity;
uint32_t resetPeriod = 250;
// reply times (same on both sides for symm. ranging)
uint16_t replyDelayTimeUS = 3000;
void setup() {
// DEBUG monitoring
Serial.begin(9600);
SPI.begin(SPI_SCK, SPI_MISO, SPI_MOSI);
Serial.println(F("### DW1000-arduino-ranging-tag ###"));
// initialize the driver
DW1000.begin(PIN_IRQ, PIN_RST);
DW1000.select(PIN_SS);
Serial.println("DW1000 initialized ...");
// general configuration
DW1000.newConfiguration();
DW1000.setDefaults();
DW1000.setDeviceAddress(2);
DW1000.setNetworkId(10);
DW1000.enableMode(DW1000.MODE_LONGDATA_RANGE_LOWPOWER);
DW1000.commitConfiguration();
Serial.println(F("Committed configuration ..."));
// DEBUG chip info and registers pretty printed
char msg[128];
DW1000.getPrintableDeviceIdentifier(msg);
Serial.print("Device ID: "); Serial.println(msg);
DW1000.getPrintableExtendedUniqueIdentifier(msg);
Serial.print("Unique ID: "); Serial.println(msg);
DW1000.getPrintableNetworkIdAndShortAddress(msg);
Serial.print("Network ID & Device Address: "); Serial.println(msg);
DW1000.getPrintableDeviceMode(msg);
Serial.print("Device mode: "); Serial.println(msg);
// attach callback for (successfully) sent and received messages
DW1000.attachSentHandler(handleSent);
DW1000.attachReceivedHandler(handleReceived);
// anchor starts by transmitting a POLL message
receiver();
transmitPoll();
noteActivity();
}
void noteActivity() {
// update activity timestamp, so that we do not reach "resetPeriod"
lastActivity = millis();
}
void resetInactive() {
// tag sends POLL and listens for POLL_ACK
expectedMsgId = POLL_ACK;
transmitPoll();
noteActivity();
}
void handleSent() {
// status change on sent success
sentAck = true;
}
void handleReceived() {
// status change on received success
receivedAck = true;
}
void transmitPoll() {
DW1000.newTransmit();
DW1000.setDefaults();
data[0] = POLL;
DW1000.setData(data, LEN_DATA);
DW1000.startTransmit();
}
void transmitRange() {
DW1000.newTransmit();
DW1000.setDefaults();
data[0] = RANGE;
// delay sending the message and remember expected future sent timestamp
DW1000Time deltaTime = DW1000Time(replyDelayTimeUS, DW1000Time::MICROSECONDS);
timeRangeSent = DW1000.setDelay(deltaTime);
timePollSent.getTimestamp(data + 1);
timePollAckReceived.getTimestamp(data + 6);
timeRangeSent.getTimestamp(data + 11);
DW1000.setData(data, LEN_DATA);
DW1000.startTransmit();
Serial.print("Expect RANGE to be sent @ "); Serial.println(timeRangeSent.getAsFloat());
}
void receiver() {
DW1000.newReceive();
DW1000.setDefaults();
// so we don't need to restart the receiver manually
DW1000.receivePermanently(true);
DW1000.startReceive();
}
void loop() {
if (!sentAck && !receivedAck) {
// check if inactive
if (millis() - lastActivity > resetPeriod) {
resetInactive();
}
return;
}
// continue on any success confirmation
if (sentAck) {
sentAck = false;
byte msgId = data[0];
if (msgId == POLL) {
DW1000.getTransmitTimestamp(timePollSent);
Serial.print("Sent POLL @ "); Serial.println(timePollSent.getAsFloat());
} else if (msgId == RANGE) {
DW1000.getTransmitTimestamp(timeRangeSent);
noteActivity();
}
}
if (receivedAck) {
receivedAck = false;
// get message and parse
DW1000.getData(data, LEN_DATA);
byte msgId = data[0];
if (msgId != expectedMsgId) {
// unexpected message, start over again
Serial.print("Received wrong message # "); Serial.println(msgId);
expectedMsgId = POLL_ACK;
transmitPoll();
return;
}
if (msgId == POLL_ACK) {
DW1000.getReceiveTimestamp(timePollAckReceived);
expectedMsgId = RANGE_REPORT;
transmitRange();
noteActivity();
} else if (msgId == RANGE_REPORT) {
expectedMsgId = POLL_ACK;
float curRange;
memcpy(&curRange, data + 1, 4);
transmitPoll();
noteActivity();
} else if (msgId == RANGE_FAILED) {
expectedMsgId = POLL_ACK;
transmitPoll();
noteActivity();
}
}
}
#include <SPI.h>
#include <DW1000.h>
// connection pins
#define SPI_SCK 18
#define SPI_MISO 19
#define SPI_MOSI 23
#define DW_CS 4
// connection pins
const uint8_t PIN_RST = 27; // reset pin
const uint8_t PIN_IRQ = 34; // irq pin
const uint8_t PIN_SS = 4; // spi select pin
// messages used in the ranging protocol
// TODO replace by enum
#define POLL 0
#define POLL_ACK 1
#define RANGE 2
#define RANGE_REPORT 3
#define RANGE_FAILED 255
// message flow state
volatile byte expectedMsgId = POLL;
// message sent/received state
volatile boolean sentAck = false;
volatile boolean receivedAck = false;
// protocol error state
boolean protocolFailed = false;
// timestamps to remember
DW1000Time timePollSent;
DW1000Time timePollReceived;
DW1000Time timePollAckSent;
DW1000Time timePollAckReceived;
DW1000Time timeRangeSent;
DW1000Time timeRangeReceived;
// last computed range/time
DW1000Time timeComputedRange;
// data buffer
#define LEN_DATA 16
byte data[LEN_DATA];
// watchdog and reset period
uint32_t lastActivity;
uint32_t resetPeriod = 250;
// reply times (same on both sides for symm. ranging)
uint16_t replyDelayTimeUS = 3000;
// ranging counter (per second)
uint16_t successRangingCount = 0;
uint32_t rangingCountPeriod = 0;
float samplingRate = 0;
void setup() {
// DEBUG monitoring
Serial.begin(9600);
delay(1000);
SPI.begin(SPI_SCK, SPI_MISO, SPI_MOSI);
Serial.println(F("### DW1000-arduino-ranging-anchor ###"));
// initialize the driver
DW1000.begin(PIN_IRQ, PIN_RST);
DW1000.select(PIN_SS);
Serial.println(F("DW1000 initialized ..."));
// general configuration
DW1000.newConfiguration();
DW1000.setDefaults();
DW1000.setDeviceAddress(1);
DW1000.setNetworkId(10);
DW1000.enableMode(DW1000.MODE_LONGDATA_RANGE_LOWPOWER);
DW1000.commitConfiguration();
Serial.println(F("Committed configuration ..."));
// DEBUG chip info and registers pretty printed
char msg[128];
DW1000.getPrintableDeviceIdentifier(msg);
Serial.print("Device ID: "); Serial.println(msg);
DW1000.getPrintableExtendedUniqueIdentifier(msg);
Serial.print("Unique ID: "); Serial.println(msg);
DW1000.getPrintableNetworkIdAndShortAddress(msg);
Serial.print("Network ID & Device Address: "); Serial.println(msg);
DW1000.getPrintableDeviceMode(msg);
Serial.print("Device mode: "); Serial.println(msg);
// attach callback for (successfully) sent and received messages
DW1000.attachSentHandler(handleSent);
DW1000.attachReceivedHandler(handleReceived);
// anchor starts in receiving mode, awaiting a ranging poll message
receiver();
noteActivity();
// for first time ranging frequency computation
rangingCountPeriod = millis();
}
void noteActivity() {
// update activity timestamp, so that we do not reach "resetPeriod"
lastActivity = millis();
}
void resetInactive() {
// anchor listens for POLL
expectedMsgId = POLL;
receiver();
noteActivity();
}
void handleSent() {
// status change on sent success
sentAck = true;
}
void handleReceived() {
// status change on received success
receivedAck = true;
}
void transmitPollAck() {
DW1000.newTransmit();
DW1000.setDefaults();
data[0] = POLL_ACK;
// delay the same amount as ranging tag
DW1000Time deltaTime = DW1000Time(replyDelayTimeUS, DW1000Time::MICROSECONDS);
DW1000.setDelay(deltaTime);
DW1000.setData(data, LEN_DATA);
DW1000.startTransmit();
}
void transmitRangeReport(float curRange) {
DW1000.newTransmit();
DW1000.setDefaults();
data[0] = RANGE_REPORT;
// write final ranging result
memcpy(data + 1, &curRange, 4);
DW1000.setData(data, LEN_DATA);
DW1000.startTransmit();
}
void transmitRangeFailed() {
DW1000.newTransmit();
DW1000.setDefaults();
data[0] = RANGE_FAILED;
DW1000.setData(data, LEN_DATA);
DW1000.startTransmit();
}
void receiver() {
DW1000.newReceive();
DW1000.setDefaults();
// so we don't need to restart the receiver manually
DW1000.receivePermanently(true);
DW1000.startReceive();
}
void computeRangeAsymmetric() {
// asymmetric two-way ranging (more computation intense, less error prone)
DW1000Time round1 = (timePollAckReceived - timePollSent).wrap();
DW1000Time reply1 = (timePollAckSent - timePollReceived).wrap();
DW1000Time round2 = (timeRangeReceived - timePollAckSent).wrap();
DW1000Time reply2 = (timeRangeSent - timePollAckReceived).wrap();
DW1000Time tof = (round1 * round2 - reply1 * reply2) / (round1 + round2 + reply1 + reply2);
// set tof timestamp
timeComputedRange.setTimestamp(tof);
}
void computeRangeSymmetric() {
// symmetric two-way ranging (less computation intense, more error prone on clock drift)
DW1000Time tof = ((timePollAckReceived - timePollSent) - (timePollAckSent - timePollReceived) +
(timeRangeReceived - timePollAckSent) - (timeRangeSent - timePollAckReceived)) * 0.25f;
// set tof timestamp
timeComputedRange.setTimestamp(tof);
}
void loop() {
int32_t curMillis = millis();
if (!sentAck && !receivedAck) {
// check if inactive
if (curMillis - lastActivity > resetPeriod) {
resetInactive();
}
return;
}
// continue on any success confirmation
if (sentAck) {
sentAck = false;
byte msgId = data[0];
if (msgId == POLL_ACK) {
DW1000.getTransmitTimestamp(timePollAckSent);
noteActivity();
}
}
if (receivedAck) {
receivedAck = false;
// get message and parse
DW1000.getData(data, LEN_DATA);
byte msgId = data[0];
if (msgId != expectedMsgId) {
// unexpected message, start over again (except if already POLL)
protocolFailed = true;
}
if (msgId == POLL) {
// on POLL we (re-)start, so no protocol failure
protocolFailed = false;
DW1000.getReceiveTimestamp(timePollReceived);
expectedMsgId = RANGE;
transmitPollAck();
noteActivity();
}
else if (msgId == RANGE) {
DW1000.getReceiveTimestamp(timeRangeReceived);
expectedMsgId = POLL;
if (!protocolFailed) {
timePollSent.setTimestamp(data + 1);
timePollAckReceived.setTimestamp(data + 6);
timeRangeSent.setTimestamp(data + 11);
// (re-)compute range as two-way ranging is done
computeRangeAsymmetric(); // CHOSEN RANGING ALGORITHM
transmitRangeReport(timeComputedRange.getAsMicroSeconds());
float distance = timeComputedRange.getAsMeters() - 0.7;
Serial.print("Range: "); Serial.print(distance); Serial.print(" m");
Serial.print(" \t RX power: "); Serial.print(DW1000.getReceivePower()); Serial.print(" dBm");
Serial.print(" \t Sampling: "); Serial.print(samplingRate); Serial.println(" Hz");
Serial.print(" FP power is [dBm]: "); Serial.print(DW1000.getFirstPathPower());
Serial.print(" RX power is [dBm]: "); Serial.print(DW1000.getReceivePower());
Serial.print(" Receive quality: "); Serial.println(DW1000.getReceiveQuality());
// update sampling rate (each second)
successRangingCount++;
if (curMillis - rangingCountPeriod > 1000) {
samplingRate = (1000.0f * successRangingCount) / (curMillis - rangingCountPeriod);
rangingCountPeriod = curMillis;
successRangingCount = 0;
}
}
else {
transmitRangeFailed();
}
noteActivity();
}
}
}
addaded resistor on bus - right now I don’t rememmber - pull up or pull down