Does the double (or float) potentially do any Mantissa rounding?

Does the double (or float) potentially do any Mantissa rounding?

Len

isnt it more like truncation?

Hi,

I’m familiar with other uses of float where a float number (after a computation) that yields a 12345678.9999999999999 results rounds up to 12345679.

The reason for the question: I’ve got a CBock with a uint64 output. The output value can use about 52 the bits of the uint64. If I use the out value in a Bsource equation, do I lose any of the bits in Mantissa rounding?