Disabling PA in MAUWBS3CA1 (MaUWB-DW3000 = DW3000 + STM32)

Hi,
I’m using “MaUWB_DW3000 with ESP32S3 AT Command” module (MAUWBS3CA1) from Makerfabs that includes a PA.
Do you know if there is any way to disable the PA ? via ESP32 AT command ?

5:19:12.269 → System Parameter
15:19:12.269 → UWB Module Compile:17:19:38 Sep 23 2024
15:19:12.269 → UWB Module Software:v01_01_001
15:19:12.269 → UWB Module Hardware:v01_03_000
15:19:12.269 → UWB Module Flag:AAAA
15:19:12.269 → UWB Module BootT:2
15:19:12.300 → UWB Module Error_Bit1:0, Error_Bit2:0, Error_Bit3:0, Error_Bit4:0, Error_Bit5:0
15:19:12.300 → UWB Module Role:Tag, Id:1, Rate:6.8M, Filter:1, AntTx:16336, AutoRpt:1, PA:1, Power:FD, ExtMode:1, slotsNum10, slotPeriod:10

Regards

Hi @farid,

This module and the FW are third-party products. So, we don’t know the command to disable the PA. I would suggest you ask Makerfabs to get an answer to your question.

Kind regards,
Emre

Hi Emre,

Thanks for your reply.
This is exactly what I did and this feature is not available in there current FW.

Regards
Farid