I can plot the current through a device by clicking on center of its symbol on the schematic. In LTspice, there was an arrow that would pop up to indicate the direcition of positive current. How can I tell the direction of positive current when in QSPICE?
1 Like
For two-terminal components, you can point at a pin instead of the body. That will plot the current into that pin.
The sign is different depending on which end of a resistor you point at.
4 Likes
How can I tell which direction the current is going if the sign of the current direction depends on which end of the component I use? If there are more than 1 dc voltages then what? I can do it mathematically but how do I find the loop currents on the schematic diagram.
@coop Does this post answer your question?
https://forum.qorvo.com/t/same-circuit-not-work-in-qspice-but-in-ltspice-worked-fine/18844/8
1 Like