Difficulty flashing FreeRTOS QANI firmware onto DWM3001CDK board

Hello, I am having a lot of trouble flashing the DWM3001CDK-QANI-FreeRTOS.hex onto my DWM3001CDK board. I have been able to successfully flash both DWM3001CDK-CLI-FreeRTOS and DWM3001CDK-UCI-FreeRTOS using JFlashLite through the J9 port and then switching to the J20 port to actually observe the output and I’ve followed all the instruction in the documentation. I have also tried using an older version of JFlashLite to no avail. Currently JFlashLite confirms a successful flashing, but when I switch to the J20 port I get a flashing red LED which signals nothing has been flashed. Any help would be appreciated. Thanks!

Hi @lhar33 !

QANI doesn’t make use of J20. Its log output is over RTT, which also uses J-Link so, after flashing, you should keep the DWM3001CDK plugged to J9 and open the J-Link RTT Viewer app.

Kind regards!

Thank you @carlos.silva that worked! I’m running into another issue, and I’m wondering whether you know the answer:
I’m trying to use apple nearby interaction (NI) in an app I am building. Currently, I’m just trying to establish a connection and tranfer of information between the board and my app. The app can discover and connect to the board over BLE, but as soon as the NI session begins the app reports NIERROR_INVALID_CONFIGURATION_DESCRIPTION, and no distance data is delivered even though it works with Qorvo’s demo app.

I’m wondering if you know what causes this and what configuration or data exchange step is required to make the NI session valid. Any help is welcomed.

Thank you!

Hi @lhar33 !

I recommend you take a look at the DW3_QM33_SDK_1.1.1/SDK/Documentation/DeveloperManual/DWM3001CDK_Developer_Manual_QM33SDK-1.1.1.pdf, check the session 12.5.3 BLE Folder.
I didn’t find an error flag NIERROR_INVALID_CONFIGURATION_DESCRIPTION, but it seems an invalid configuration during the OOB “handshake”. Adding breakpoints to both iOS and the device app may help.
If you need more info on the data exchange, the older QANI versions have a good explanation in their “Accessory Developer Guide”, these older releases are available here: https://www.qorvo.com/products/d/da008212

The implementation is different from the DW3/QM33 SDK, but the communication flow explained there is the same.

Kind regards!

Did you look at the sample app code in the QANI sdk
It shows the OOB protocol that Qorvo uses

After connect it send a 1 byte init command
The device sends back the configuration

Later the phone app merges the config with the app side
Starts ranging with it and sends it to the device
Which starts ranging too.

Our app is written in ionic and I wrote a plugin that goes all the same work as the sample app