Hello,
Maybe one can figure out where is the mistake:
tes3.qsch (47.5 KB)
The correct ones are results with G_S14_2, etc, so with 2:
They are looking the same:
But I do not know why I am receiving different results though as you can see from above the signals are the same:
With G_S14_2, G_S23_2. G_S58_2 and G_S67_2:
With G_S14_1, G_S23_1. G_S58_1 and G_S67_1:
To be at the beginning, although after the first period the signals become ok: