Hi Mike,
In the current QSPICE GUI implementation, the output window also contains the measurement results of the .meas commands called from the schematic page. Would it be possible to display this information at the top in the measurement window below the waveform viewer instead, so that additional trace measurements could be appended to it?
Also, it would be very handy if the context menu in the measurement window could be extended by the option to clear selected measurement results, instead of clearing the entire content of the measurement window as it is currently implemented via “Clear this window or text”.
Many thanks,
Georg