Hi,
I just tried testing Dflop in both SPICEs, and see the response to PRE and CLR are different. Please see the waveform below. Any comments why is that?
Thanks!
Yi
Hi,
I just tried testing Dflop in both SPICEs, and see the response to PRE and CLR are different. Please see the waveform below. Any comments why is that?
Thanks!
Yi
A long time ago on the LTspce forum it was discovered that the CD4013 model is somewhat defective. This was also discussed on the Russian forum. As a rule, this is not noticeable. Perhaps Qspice decided to fix this.
Here is the CD4013 schematic:

Hi Bordoynov,
Have checked the function table of CD4013B. See below:
And what happens when you change SET and RESET to low at the same time ?
Is there right and wrong if both SET and RESET equals 1 for D-type flip-flop?
SET (PRE) represent to force Output Q to 1
RESET (CLR) represent to force Output Q to 0
Setting both SET and RESET to 1 is defined as Illegal concurrent, some will call it forbidden state.
I change SET and RESET to go up and down at the same time:
Kelvin, you are right. Just wondering why LTSPICE and QSPICE gives different results when both are high. They are both developed by Mike…
I think you can contact Mike to review if it worth a change if you truly have a need for Q to be 1 when both RESET and SET are high and for this logic to match CD4013.
Qspice does not include the LTspice A-device, which is Analog Device IP. This could be why the logic devices in Qspice do not follow A-device logic.
However, since RESET=SET=1 is typically considered not to be used, and different simulators implement their responses differently, it’s uncertain if anything needs to be done about that. Alternatively, you can actually use C++ to write a D flip-flop that provides such a response. There are no limitations on how logic is implemented with the support of a C++ block.
You should consider Qspice as something entirely new. For example, something in LTspice that is regarded as good but not implemented in Qspice may be seen as bad (e.g., L in capacitor model, modified Trap integration).
See 74HC74:

This is an example to use C++ block to implement a D-flop with CD4013B logic table. I hope I didn’t make a mistake here.
D-flop-CD4013B.qsym (904 Bytes)
d_flop_cd4013b.cpp (3.4 KB)
D-FLOP-CD4013B - Truth Table.qsch (6.7 KB)
Hi Kelvin,
Really appreciate your effort and explanation up there.
The logic in the C++ file looks right to me.
Thanks, the logic looks the same to CD4013 and the footnote is clear.
I have an opportunity revisit this case and built a D-flop with logic table as CD4013B with Qspice native device (last time I proposed a C++ block). This can eliminate the need of having .dll to support the simulation.
D-flop-CD4013B.qsym (1.5 KB)
example.D-flop-CD4013B.qsch (10.9 KB)
This example compare default Qspice D-flop and this CD4013B logic table D-flop. The different is during both SET and RESET are HIGH.