I have two computers with QSpice loaded. Both computers are running Windows 10.
QSpice is working well on both systems. I tend to launch QSpice from the QSpice icon I attached to the TaskBar.
However I noticed a difference between the two computers in this regards.
On one computer, if I “Right Click” on the QSpice icon, I get a list of the latest .qsch projects I had previously run. I can then select one and launch that sim.
On the other computer, I do not get the list of previously run sim projects. Note: Using other other apps I’ve attached to the Taskbar of this computer, if I “Right Click” I will get a list of previously run files/projects. Additionally, I have uninstalled QSpice multiple times and installed as “User” and “Admin”. Still no change.
Is there a setting I am missing?
Len